This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: What is ADC Internal impedance value?

Part Number: AM3352

Hi Expert,

What is ADC Internal impedance value?

I can not find out the data from datasheet.

How do I to get the value?

Thanks

Daniel

  • Are you asking for input impedance looking into one of the AIN pins of the ADC?  If so, that is defined in the datasheet.

    Input impedance of AIN[7:0], when ƒ = frequency of applied signal: [1 / ((65.97 × 10E–12) × ƒ)] Ω.

    This defines the dynamic input impedance. 

    The input could also have about 1uA of leakage current as the applied voltage approaches VDDA_ADC or VSS_ADC, where the AIN pin sources current when the voltage applied is less than mid-supply and the AIN pin sinks current when the voltage applied is greater than mid-supply.

    Regards,
    Paul