This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error "can't locate the package 'ti.sdo.ce.osal' along the path"



Hi,

I am trying to build a iUniversial type application. I successfully generated and packaged my own CODEC (via the CODEC package generation Wizard) and a server (via the server package generation Wizard). Next I created an application (reused the code and structure of randgen from the iUNIVERSAL examples as suggested by the documentation). I hit the same issue with my own application and also with the iUNIVERSIAL examples' applications: randgen and fir in which packages under the code engine directories are not found. I guess the problem is path issue and indeed the -Dxdc_path printed on the Linux monitor states the XDC install directory only (in addition to /../../ etc). I did set in the Makefile the XDCPATH to include also code_engine/packages and code_engine/cetools and other directories but still it did not help.

Thanks Ofer