Part Number: PROCESSOR-SDK-AM437X
Other Parts Discussed in Thread: AM4378
Hello,
I have a custom board with AM4378 connected to OV2640. I'm using SDK5.3 and am not able to get the camera working. When I start a gstreamer pipeline or the dual_camera demo, I get the error -
vpfe 48328000.vpfe: Error in attaching interrupt handle
I see this print in the vpfe_start_streaming function. What could be causing this issue?
The device tree entries and the hardware schematic for the camera portion are very similar to the GP EVM. The relevant extracts -
// Under am43xx_pinmux
cam1_pins_default: cam1_pins_default {
pinctrl-single,pins = <
0x1dc ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AE21) cam1_pclk.cam1_pclk */
0x1d4 ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AD25) cam1_hsync.cam1_hsync */
0x1d8 ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AC23) cam1_vsync.cam1_vsync */
0x1e8 ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AB20) cam1_data0.cam1_data0 */
0x1ec ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AC21) cam1_data1.cam1_data1 */
0x1f0 ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AD21) cam1_data2.cam1_data2 */
0x1f4 ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AE22) cam1_data3.cam1_data3 */
0x1f8 ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AD22) cam1_data4.cam1_data4 */
0x1fc ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AE23) cam1_data5.cam1_data5 */
0x200 ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AD23) cam1_data6.cam1_data6 */
0x204 ( PIN_INPUT_PULLUP | MUX_MODE0 ) /* (AE24) cam1_data7.cam1_data7 */
>;
};
// Under i2c0
ov2640: camera@30 {
compatible = "ovti,ov2640";
reg = <0x30>;
status = "okay";
resetb-gpios = <&gpio4 13 GPIO_ACTIVE_LOW>;
clocks = <&audio_mstrclk>;
clock-names = "xvclk";
port {
ov2640_0: endpoint {
remote-endpoint = <&vpfe1_ep>;
};
};
};
&vpfe1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&cam1_pins_default>;
port {
vpfe1_ep: endpoint {
remote-endpoint = <&ov2640_0>;
ti,am437x-vpfe-interface = <0>;
bus-width = <8>;
hsync-active = <0>;
vsync-active = <0>;
};
};
};