Part Number: TDA4VM
On TDA4VM, when Linux boots up, there are two consoles, one on UART0 and another on UART1. they are ttyS2, ttyS3 respectively. How can I disable ttyS3 been used as a console, 'cause I want to use it as a general UART device.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
On TDA4VM, when Linux boots up, there are two consoles, one on UART0 and another on UART1. they are ttyS2, ttyS3 respectively. How can I disable ttyS3 been used as a console, 'cause I want to use it as a general UART device.
In fact, there are services that will start two consoles when tty devices avaliable. I disabled one of those services and now I have only one console. Don't know why TI put this in the root file system.