This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: Cache coherency with DMA masters and other processors (R5f, PRUs)

Part Number: AM6442


Dear TI team,

we've finally realized that on the AM65x the A53's caches are not coherent with accesses from the R5f (see related thread).

We're working on several designs spanning multiple TI processors, including the AM64x.

In that thread explained that the AM64x is cache coherent via its ACP port, unlike the AM65x, where coherence is achieved via the MSMC and the northbridge (NB).

Unfortunately the AM64x TRM is still rather sparse on details, and apparently doesn't cover this topic at all. As far as I understand the ACP provides a means for an uncached master (e.g. DMA) to access memory via the ACP, so that the accesses pass by the A53's L2 memory system, thus ensuring coherence. How is this implemented on the AM64x?

Do all accesses by uncached masters go through the ACP?

How can we control which accesses go through the ACP?

Regards,

Dominic

  • Dominic,

    Thanks for working through the issues with AM65x and coherency, unfortunately resulting in the clarification the R5 access will not be coherent with A53 caches. On AM64x the approach to coherency is much simpler and is controlled by the initiator/master setting a bus value called asel (address selector) to decide if the read/write is non-coherent, or if it gets routed through the A53 ACP port for coherency. The asel values are:

    Write transaction with asel=14 ,cause L2 cache allocation: for cache warming feature

    Write transactions with asel=15, does not cause L2 cache allocation

    Read transactions with asel=14 and 15, does not cause L2 cache allocation

    asel = 0 is a non-coherent transaction. This feature is used in Linux DMA driver and is measured to result in 10-25% performance lift at the iperf3 or netperf level benchmarks with Ethernet (cpsw3g). Asel can be set per DMA channel and per initiator like R5. Unfortunately it looks like the TRM section is lacking these details. I will add some of the details to this post and file some documentation bugs to get the TRM updated but wanted to get this initial response first. If you search the TRM for asel you'll find couple DMA channel setups for this, without the bits defined the four bits are as above (legal values 0, 14, 15).

      Pekka

  • Hello Pekka,

    thanks for this explanation, that really helps.

    I already saw the few places where ASEL is mentioned, but the TRM definitely could use an update in that area (among others... ). For now it would be great if you could post the details here.

    Regards,

    Dominic

  • I've found the details and they will be in the next TRM revision. But while waiting for that here is a compressed version. The register QoS_MAP to modify looks like:

    Bit

    Name

    Type

    Reset

    Description

    31:30

    reserved

    r

    0x0

    Reserved

    29:28

    atype

    rw

    0x0

    atype signal for channel N. 0 = physical. 1 = intermediate. 2 = virtual. 3 = physical with coherence.

    27:16

    virtid

    rw

    0x0

    virtid signal for channel N.

    15

    reserved

    r

    0x0

    Reserved

    14:12

    epriority

    rw

    0x7

    epriority signal for channel N.

    11:8

    asel

    rw

    0x0

    asel signal for channel N. 0 = SOC address. 14  for ACP cache allocate, 15 for ACP do not allocate.

    7:4

    orderid

    rw

    0x0

    orderid signal for channel N.

    3

    reserved

    r

    0x0

    Reserved

    2:0

    qos

    rw

    0x0

    qos signal for channel N.

    These start at base address 0x45D0 0000. For each R5 there is a separate read and write port for a total of 8 of these registers (will be in Table 3-14 in TRM). Formula for the base address is 0x45d0 0000+QoS_MAP_index*0x400+0x100. The QoS_MAP_index 's are: below. R5 core 0 read port is is 0x45d00000+(522*0x400)+0x100 = 0x45d82900. I tested a couple and the values look like reset value of 0x00007000. And all of these should work with ACP.

    Port QoS index Address
    R5_core0.rmst0 522 0x45d82900
    R5_core0.wmst0 523 0x45d82d00
    R5_core1.wmst1 527
    R5_core1.rmst1 528
    R5_core2.rmst0 532
    R5_core2.wmst0 533
    R5_core3.wmst1 537
    R5_core3.rmst1 538
    PCIe read 544
    PCIe write 545

      Pekka