Part Number: PROCESSOR-SDK-AM437X
Hello
i am getting this error while running bit bake please help me out.
[user@localhost build]$ MACHINE=am57xx-evm bitbake arago-base-tisdk-image
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
WARNING: Layer meta-processor-sdk should set LAYERSERIES_COMPAT_meta-processor-sdk in its conf/layer.conf file to list the core layer names it is compatible with.
Loading cache: 100% |############################################| Time: 0:00:02
Loaded 4658 entries from dependency cache.
WARNING: No recipes available for:
/home/user/sitara/tisdk/sources/meta-arago/meta-arago-distro/recipes-browser/chromium/chromium-wayland_%.bbappend
/home/user/sitara/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/move-base_1.12.14.bbappend
/home/user/sitara/tisdk/sources/meta-processor-sdk/recipes-ros/navigation/rotate-recovery_1.12.14.bbappend
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.40.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "centos-7"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am57xx-evm"
DISTRO = "arago"
DISTRO_VERSION = "2019.11"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:56d9d47f18eeec31a1086ca29e54b5956c46de84"
meta-aws = "HEAD:6432f1b38b9dcbbb55020167f5b1cfe55e858c6d"
meta-ros = "HEAD:72068b17e4192b51e09c8dc633805a35edac8701"
meta-arago-distro
meta-arago-extras = "HEAD:70436496d2617b281c51390faa3d421814055cd6"
meta-browser = "HEAD:5f365ef0f842ba4651efe88787cf9c63bc8b6cb3"
meta-qt5 = "HEAD:e6e464c9ed9266ce46452f953c1bdcb0e7b2d95f"
meta-virtualization = "HEAD:7685c7d415e0002c448007960837ae8898cd57a5"
meta-networking
meta-python
meta-oe
meta-gnome
meta-multimedia
meta-filesystems = "HEAD:446bd615fd7cb9bc7a159fe5c2019ed08d1a7a93"
meta-ti = "HEAD:b27317ab4f9be931a66344ca502c7e3f4ec780e5"
meta-linaro-toolchain
meta-optee = "HEAD:615ea7561b844a3867cee4299d83d605c10b02ab"
meta = "HEAD:e68991ceb5933f7d03b96697e8a0ba0829feb320"
Initialising tasks: 100% |#######################################| Time: 0:00:06
Sstate summary: Wanted 1452 Found 0 Missed 1452 Current 85 (0% match, 5% complete)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: ti-cgt-pru-native-2.3.2-r0 do_fetch: Failed to fetch URL software-dl.ti.com/.../ti_cgt_pru_2.3.2_linux_installer_x86.bin;name=cgt-pru-x86, attempting MIRRORS if available
ERROR: ti-cgt-pru-native-2.3.2-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-iZ8UcvCwJ1,guid=1deb0b84378d9f0d7ac4be9360641760"; export SSH_AGENT_PID="8388"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export https_proxy="">my.proxy.com:port_number"; export PATH="/home/user/sitara/tisdk/sources/oe-core/scripts/native-intercept:/home/user/sitara/tisdk/sources/oe-core/scripts:/home/user/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/ti-cgt-pru-native/2.3.2-r0/recipe-sysroot-native/usr/bin/x86_64-linux:/home/user/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/ti-cgt-pru-native/2.3.2-r0/recipe-sysroot-native/usr/bin:/home/user/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/ti-cgt-pru-native/2.3.2-r0/recipe-sysroot-native/usr/sbin:/home/user/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/ti-cgt-pru-native/2.3.2-r0/recipe-sysroot-native/usr/bin:/home/user/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/ti-cgt-pru-native/2.3.2-r0/recipe-sysroot-native/sbin:/home/user/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/ti-cgt-pru-native/2.3.2-r0/recipe-sysroot-native/bin:${DEF_TOOLCHAIN_PATH}/bin:/home/user/sitara/tisdk/sources/bitbake/bin:/home/user/sitara/tisdk/build/arago-tmp-external-arm-toolchain/hosttools"; export HOME="/home/user"; /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /home/user/sitara/tisdk/downloads 'software-dl.ti.com/.../ti_cgt_pru_2.3.2_linux_installer_x86.bin' --progress=dot -v failed with exit code 8, output:
--2021-03-31 09:47:41-- software-dl.ti.com/.../ti_cgt_pru_2.3.2_linux_installer_x86.bin
Resolving software-dl.ti.com (software-dl.ti.com)... 104.121.232.201, 2600:1417:73:4b0::b48, 2600:1417:73:4a9::b48
Connecting to software-dl.ti.com (software-dl.ti.com)|104.121.232.201|:80... connected.
HTTP request sent, awaiting response... 302 Moved Temporarily
Location: www.ti.com/.../anonymousproddownload.tsp [following]
Error parsing proxy URL my.proxy.com:port_number: Bad port number.
ERROR: ti-cgt-pru-native-2.3.2-r0 do_fetch: Fetcher failure for URL: 'software-dl.ti.com/.../ti_cgt_pru_2.3.2_linux_installer_x86.bin;name=cgt-pru-x86'. Unable to fetch URL from any source.
ERROR: ti-cgt-pru-native-2.3.2-r0 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/user/sitara/tisdk/build/arago-tmp-external-arm-toolchain/work/x86_64-linux/ti-cgt-pru-native/2.3.2-r0/temp/log.do_fetch.27243
ERROR: Task (virtual:native:/home/user/sitara/tisdk/sources/meta-ti/recipes-ti/devtools/ti-cgt-pru_2.3.2.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 979 tasks of which 974 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
virtual:native:/home/user/sitara/tisdk/sources/meta-ti/recipes-ti/devtools/ti-cgt-pru_2.3.2.bb:do_fetch
Summary: There were 4 WARNING messages shown.
Summary: There were 3 ERROR messages shown, returning a non-zero exit code.
[user@localhost build]$