Hi All,
I would like to ask one question on reset supervisor’s configuration for DM6437.

In EVM6437 schematics sheet 33 – Reset Supervisor, what is the purpose of the diode D10? Since D10 pass only higher voltage of its pin 1 respective to 3, then when U57 is asserts low, the low voltage signal cannot be passed to U56’s MRn pin, which renders the cascading ineffective.
So why D10 is still placed here? Can I remove it?
Another question is on EMU_SYS_RESETn signal. Its receiving end is pin PONRSn of EVM6437’s emulation USB which is proprietary to SpectrumDigital, so I have no idea of its internal operation. But from the schematics it seems that EMU_SYS_RESETn and RESETn probably related in that the former triggers the later, is it the case?
Thanks,
Zheng