This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-K2G: Issue building the Big Data IPC example

Part Number: PROCESSOR-SDK-K2G


I have installed both Linux and RTOS processor SDKs for K2G (both are version 6_01_00_08) and am trying to build the big data IPC example for the case where the host is running Linux. The readme file in the processor_sdk_rtos/demos/bigdataipc directory says that the examples are integrated into the top level make of the Linux SDK, however I cannot find the right command to build this example. I would greatly appreciate any suggestions.