Part Number: TMDX654IDKEVM
We are trying to interface the AM65x with a Sony IMX264 camera sensor. We are lead to believe this should work but I am uncertain what the Start and End frame codes should be because the Sony datasheet doesn't specify start or end of frame codes. Are you able to confirm if this should work and if so what the setting need to be?
When I run my code using the Sony line invalid codes (see Sony sync codes below) for the SoF\EoF I receive and raw IRQ EOX not received. I assume EOX means end of frame.