This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: gstreamer pipeline memory leak

Part Number: AM5728

I use processor sdk 04_03_00_05 in my am5728 board。


And I have a gstreamer pipeline "filesrc ! qtdemux ! h264parse ! ducatih264dec ! vpe ! appsink" in my application。

But when I start the pipeline and then rease it again and again, I found memory leak。

what I only do in appsrc for debuging  is mapping the buffer and then unmap it。it's also memory leak.

  • Hi Yin Deng,

    Is this issue reproduced on the TI EVM or your custom hardware?

    If it is on the TI EVM then I request you to try it on the latest version of the SDK 06.03.00.106 and see if you can recreate the same. Unfortunately the SDK version 04.03.00.05 is very old and is not actively supported.

    Regards

    Karthik