This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DVSDK and OMAP-L137 EVM SD Card

Other Parts Discussed in Thread: OMAP-L137

I've built and programmed the Linux kernel from DVSDK 3.20.00.14 into my OMAP-L137 EVM. I get a kernel panic because /dev/mmcblk0p1 does not automatically get created. I''ve tried modifying the da830_omapl137_defconfig afterwards to match the linux-2.6.18 config with the linux-03.20.00.14 config (aka linux-2.6. 33-rc4). Can I assume that the SD Card that came with the EVM can be used with newer kernels? Is there a config option I am missing?

5074.config_dvsdk_mod6.txt

7041.capture.txt