This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3630 ZOOM3 C64+ CCS3.3 projects

I have OMAP3630 ZOOM3 board and need develop the algorithms on the C64+ inside. I need a project example of C64+ in the ZOOM3 for CCS3.3, it should incluse cmd file, c main file, some board initilization lib or functions. Would anyone please help me get it?

At same time, GEL files of the cortex and DSP for OMAP3630 are better, I only have the ones for OMAP3430.I don't know if they are same as each other.