This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA821U: Linux: ethernet eth0 link down and up messages

Part Number: DRA821U
Other Parts Discussed in Thread: DRA821

Hi,

on a DRA821 SOM/CP board setup with latest PSDK Linux 7.2, i am getting the following message every few seconds

[ 8547.002952] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
[ 8548.031143] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[ 8562.362966] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
[ 8563.387058] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[ 8643.257590] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
[ 8644.281501] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off

The MCU_ENET port is connected and works functionally.

What is the issue with that port, that it takes the link down and then up again right away?

Regards,

--Gunter