This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are using the resizeImage function from app_tidl to upscale images in the target (c66) for app_tidl_od but we find that it adds more than 100ms latency to the entire pipeline.
1. Are there ways to optimize it?
2. Does this function upscale a smaller image (30x40pixels) to a larger image (256x256)? or does it just downscale?
Regards,
Prithvi
HI,
This is plain C code, and I guess it can do up scaling and downscaling both. Definitely it can be optimized using C intrinsics of C66x DSP. Theoretical compute performance for this loop should be ~3 cycle per output leaving the border corner scenario. Since in the demo resize resolution is low (256x256) hence cycle consumed is low and so plain C code is used there without any optimization. There are many online material available for C66x optimization tricks, you may refer that for optimizing this.
Regards
Deepak Poddar