My fellows and i used DSP C6455 and FPGA chip to build a telecomunication system. And the FPGA chip is used to provide interrupts for DSP. The totall interrupt is ninty. And when DSP receives an interrupt, the program runs to an interrupt program and an interrupt accoplish program after it finished. However, two Interrupt accomplish programs were called after the first interrupt program completed. And the other 89 interrupt's accoplish program is correctlly called.