ARM side and MPEG are communicated by using DSP Bridge.
When following DLL is loaded after loading starts from the ARM side (dspexec), and the encode processing of MEPG4 was executed, the following errors generate the base image that our company makes.
Please teach what how is necessary to be thought as a cause.
Base image
DOF file DLL module usn.dll64P mp4vdec_sn.dll64P m4venc_sn.dll64P that our company makes
When you go from the ARM side in the above-mentioned in the processing of encode by way of Bridge
****************LCML ERROR : DSP ************************
Error: Create the Node : Err Num = ffffffac
****************LCML ERROR : DSP ************************
It drinks and the error occurs.
The error is a return value of the DSPNode_Create() processing. However, the cause where it is generated is uncertain. Please teach.
The dskt2 package, the ACPY3 package, the dman3 package, and the fcpy_ti64 package are built into the base image.
Moreover, EXTHEAPSIZE is increased to 0x180000.
Information such as CCS and bios is the following.
CCS : V4.2.1.00004
bios : 5.41.10.36
C6000 Code Generation Tools : 7.2.1
At the obtaining destination of the source of dspbridge:
http://www.omappedia.org/wiki/DSPBridge_Project
By Urabe