This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: The 9-port Gigabit Ethernet Switch (CPSW0) works unstable

Part Number: TDA4VM

I have repeatedly encountered that the divice which connected with  the 9-port Gigabit Ethernet Switch (CPSW0)  cannot be pinged after power-on , Will resume after ifdown up .

Could you please give us any suggestions?

Thanks

  • Hi,

    Please provide

    1. SDK version ? Linux or RTOS ?

    2. Have you made any custom changes to the code or device tree or pinmux ? Please provide that

    3. Can you provide the statistics for Ethernet ? Any packet loss ? error counters ?

    Regards

    Vineet

  • Sorry for the late reply , about your questions:

    1. SDK version is 7.2 ,LINUX.

    2. Yes ,  we do some change,  and I've shared this part of the code with TI's FAE.

    3. We have reproduced this problem together with Ti FAE, Through communication with Ti FAE, we plan to print the register when the problem is reproduced. After the problem is reproduced, I will update it.

  • Hi,

    I have tried with SDK 7.2 and TDA4 EVM, I don't face such issues. How are you pinging the CPSW 9G ? Are you assigning a static IP ? Please share the sequence.

    There is currently an issue that on Linux CPSW 9G interface cannot receive broadcast frames so you can't ping from another device first, you will have to ping from CPSW 9G and then only you can ping in other direction but going by your description you don't seem to be facing this issue.

    Regards

    Vineet

  • Hi,

        Thanks for your support.

       We have 2 boards with static IP, and the 2 boards always ping each other  for both of cpsw 9g and mcu cpsw 2g , We make sure that Ping is always done .

       I think this problem is not the same as the problem with the Ping issue ,  and we can meet this problem on mcu cpsw 2g too.  

      Regards

  • Hi,

    Is this on your custom board ? Can you confirm that you don't see the problem on EVM.

    Regards

    Vineet

  • Hi Vineet:

    At EVM board we do not reproduce this issue last week and we are try to find method reproduce at EVM board.

    Some detail information will send you through email.

    Best Regards!

    Han Tao

  • CPSW_SS_CPSW_NUSS_IDVER_REG              0x46000000: 0x6ba00101 
    CPSW_SS_SYNCE_COUNT_REG                  0x46000004: 0x0 
    CPSW_SS_SYNCE_MUX_REG                    0x46000008: 0x0 
    CPSW_SS_CONTROL_REG                      0x4600000c: 0x0 
    CPSW_SS_SGMII_MODE_REG                   0x46000010: 0x1 
    CPSW_SS_RGMII_STATUS_REG                 0x46000018: 0x0 
    CPSW_SS_SUBSSYSTEM_STATUS_REG            0x4600001c: 0x0 
    CPSW_MDIO_VERSION_REG                    0x46000f00: 0x70907 
    CPSW_MDIO_CONTROL_REG                    0x46000f04: 0x8100014c 
    CPSW_MDIO_ALIVE_REG                      0x46000f08: 0x8 
    CPSW_MDIO_LINK_REG                       0x46000f0c: 0x8 
    CPSW_MDIO_LINK_INT_RAW_REG               0x46000f10: 0x0 
    CPSW_MDIO_LINK_INT_MASKED_REG            0x46000f14: 0x0 
    CPSW_MDIO_LINK_INT_MASK_SET_REG          0x46000f18: 0x0 
    CPSW_MDIO_LINK_INT_MASK_CLEAR_REG        0x46000f1c: 0x0 
    CPSW_MDIO_USER_INT_RAW_REG               0x46000f20: 0x1 
    CPSW_MDIO_USER_INT_MASKED_REG            0x46000f24: 0x0 
    CPSW_MDIO_USER_INT_MASK_SET_REG          0x46000f28: 0x0 
    CPSW_MDIO_USER_INT_MASK_CLEAR_REG        0x46000f2c: 0x0 
    CPSW_MDIO_MANUAL_IF_REG                  0x46000f30: 0x1 
    CPSW_MDIO_POLL_REG                       0x46000f34: 0x0 
    CPSW_MDIO_POLL_EN_REG                    0x46000f38: 0xffffffff 
    CPSW_MDIO_CLAUS45_REG                    0x46000f3c: 0x0 
    CPSW_MDIO_USER_ADDR0_REG                 0x46000f40: 0x0 
    CPSW_MDIO_USER_ADDR1_REG                 0x46000f44: 0x0 
    CPSW_CPTS_IDVER_REG                      0x4603d000: 0x4e8a010a 
    CPSW_CPTS_CONTROL_REG                    0x4603d004: 0x21 
    CPSW_CPTS_RFTCLK_SEL_REG                 0x4603d008: 0x0 
    CPSW_CPTS_TS_PUSH_REG                    0x4603d00c: 0x0 
    CPSW_CPTS_TS_LOAD_VAL_REG                0x4603d010: 0xbe863d1e 
    CPSW_CPTS_TS_LOAD_EN_REG                 0x4603d014: 0x0 
    CPSW_CPTS_TS_COMP_VAL_REG                0x4603d018: 0x0 
    CPSW_CPTS_TS_COMP_LEN_REG                0x4603d01c: 0x0 
    CPSW_CPTS_INTSTAT_RAW_REG                0x4603d020: 0x0 
    CPSW_CPTS_INTSTAT_MASKED_REG             0x4603d024: 0x0 
    CPSW_CPTS_INT_ENABLE_REG                 0x4603d028: 0x1 
    CPSW_CPTS_TS_COMP_NUDGE_REG              0x4603d02c: 0x0 
    CPSW_CPTS_EVENT_POP_REG                  0x4603d030: 0x0 
    CPSW_CPTS_EVENT_0_REG                    0x4603d034: 0x0 
    CPSW_CPTS_EVENT_1_REG                    0x4603d038: 0x0 
    CPSW_CPTS_EVENT_2_REG                    0x4603d03c: 0x0 
    CPSW_CPTS_EVENT_3_REG                    0x4603d040: 0x0 
    CPSW_CPTS_TS_LOAD_HIGH_VAL_REG           0x4603d044: 0x0 
    CPSW_CPTS_TS_COMP_HIGH_VAL_REG           0x4603d048: 0x0 
    CPSW_CPTS_TS_ADD_VAL_REG                 0x4603d04c: 0x1 
    CPSW_CPTS_TS_PPM_LOW_VAL_REG             0x4603d050: 0x0 
    CPSW_CPTS_TS_PPM_HIGH_VAL_REG            0x4603d054: 0x0 
    CPSW_CPTS_TS_NUDGE_VAL_REG               0x4603d058: 0x0 
    CPSW_GENF0_COMP_LOW_REG                  0x4603d0e0: 0x0 
    CPSW_GENF0_COMP_HIGH_REG                 0x4603d0e4: 0x0 
    CPSW_GENF0_TS_GENF_CONTROL_REG           0x4603d0e8: 0x0 
    CPSW_GENF0_LENGTH_REG                    0x4603d0ec: 0x0 
    CPSW_GENF0_PPM_LOW_REG                   0x4603d0f0: 0x0 
    CPSW_GENF0_PPM_HIGH_REG                  0x4603d0f4: 0x0 
    CPSW_GENF0_NUDGE_REG                     0x4603d0f8: 0x0 
    CPSW_GENF1_COMP_LOW_REG                  0x4603d100: 0x0 
    CPSW_GENF1_COMP_HIGH_REG                 0x4603d104: 0x0 
    CPSW_GENF1_CONTROL_REG                   0x4603d108: 0x0 
    CPSW_GENF1_LENGTH_REG                    0x4603d10c: 0x0 
    CPSW_GENF1_PPM_LOW_REG                   0x4603d110: 0x0 
    CPSW_GENF1_PPM_HIGH_REG                  0x4603d114: 0x0 
    CPSW_GENF1_NUDGE_REG                     0x4603d118: 0x0 
    CPSW_ESTF1_COMP_LOW_REG                  0x4603d200: 0x0 
    CPSW_ESTF1_COMP_HIGH_REG                 0x4603d204: 0x0 
    CPSW_ESTF1_CONTROL_REG                   0x4603d208: 0x0 
    CPSW_ESTF1_LENGTH_REG                    0x4603d20c: 0x0 
    CPSW_ESTF1_PPM_LOW_REG                   0x4603d210: 0x0 
    CPSW_ESTF1_PPM_HIGH_REG                  0x4603d214: 0x0 
    CPSW_ESTF1_NUDGE_REG                     0x4603d218: 0x0 
    CPSW_CPSW_ID_VER_REG                     0x46020000: 0x6ba80100 
    CPSW_CONTROL_REG                         0x46020004: 0x6006 
    CPSW_EM_CONTROL_REG                      0x46020010: 0x0 
    CPSW_STAT_PORT_EN_REG                    0x46020014: 0x3 
    CPSW_PTYPE_REG                           0x46020018: 0x0 
    CPSW_SOFT_IDLE_REG                       0x4602001c: 0x0 
    CPSW_THRU_RATE_REG                       0x46020020: 0x3001 
    CPSW_GAP_THRESH_REG                      0x46020024: 0xb 
    CPSW_TX_START_WDS_REG                    0x46020028: 0x8 
    CPSW_EEE_PRESCALE_REG                    0x4602002c: 0x0 
    CPSW_TX_G_OFLOW_THRESH_SET_REG           0x46020030: 0xffffffff 
    CPSW_TX_G_OFLOW_THRESH_CLR_REG           0x46020034: 0x0 
    CPSW_TX_G_BUF_THRESH_SET_L_REG           0x46020038: 0xffffffff 
    CPSW_TX_G_BUF_THRESH_SET_H_REG           0x4602003c: 0xffffffff 
    CPSW_TX_G_BUF_THRESH_CLR_L_REG           0x46020040: 0x0 
    CPSW_TX_G_BUF_THRESH_CLR_H_REG           0x46020044: 0x0 
    CPSW_VLAN_LTYPE_REG                      0x46020050: 0x88a88100 
    CPSW_EST_TS_DOMAIN_REG                   0x46020054: 0x0 
    CPSW_TX_PRI0_MAXLEN_REG                  0x46020100: 0x7e8 
    CPSW_TX_PRI1_MAXLEN_REG                  0x46020104: 0x7e8 
    CPSW_TX_PRI2_MAXLEN_REG                  0x46020108: 0x7e8 
    CPSW_TX_PRI3_MAXLEN_REG                  0x4602010c: 0x7e8 
    CPSW_TX_PRI4_MAXLEN_REG                  0x46020110: 0x7e8 
    CPSW_TX_PRI5_MAXLEN_REG                  0x46020114: 0x7e8 
    CPSW_TX_PRI6_MAXLEN_REG                  0x46020118: 0x7e8 
    CPSW_TX_PRI7_MAXLEN_REG                  0x4602011c: 0x7e8 
    CPSW_P0_CONTROL_REG                      0x46021004: 0x1 
    CPSW_P0_FLOW_ID_OFFSET_REG               0x46021008: 0x30 
    CPSW_P0_BLK_CNT_REG                      0x46021010: 0x2 
    CPSW_P0_PORT_VLAN_REG                    0x46021014: 0x0 
    CPSW_P0_TX_PRI_MAP_REG                   0x46021018: 0x76543210 
    CPSW_P0_PRI_CTL_REG                      0x4602101c: 0x0 
    CPSW_P0_RX_PRI_MAP_REG                   0x46021020: 0x76543210 
    CPSW_P0_RX_MAXLEN_REG                    0x46021024: 0x5f2 
    CPSW_P0_TX_BLKS_PRI_REG                  0x46021028: 0x1245678 
    CPSW_P0_IDLE2LPI_REG                     0x46021030: 0x0 
    CPSW_P0_LPI2WAKE_REG                     0x46021034: 0x0 
    CPSW_P0_EEE_STATUS_REG                   0x46021038: 0x60 
    CPSW_P0_RX_PKTS_PRI_REG                  0x4602103c: 0x0 
    CPSW_P0_RX_GAP_REG                       0x4602104c: 0x1000000 
    CPSW_P0_FIFO_STATUS_REG                  0x46021050: 0x0 
    CPSW_P0_TX_D_THRESH_SET_L_REG            0x46021180: 0x1f1f1f1f 
    CPSW_P0_TX_D_THRESH_SET_H_REG            0x46021184: 0x1f1f1f1f 
    CPSW_P0_TX_D_THRESH_CLR_L_REG            0x46021188: 0x0 
    CPSW_P0_TX_D_THRESH_CLR_H_REG            0x4602118c: 0x0 
    CPSW_P0_TX_G_BUF_THRESH_SET_L_REG        0x46021190: 0x1f1f1f1f 
    CPSW_P0_TX_G_BUF_THRESH_SET_H_REG        0x46021194: 0x1f1f1f1f 
    CPSW_P0_TX_G_BUF_THRESH_CLR_L_REG        0x46021198: 0x0 
    CPSW_P0_TX_G_BUF_THRESH_CLR_H_REG        0x4602119c: 0x0 
    CPSW_P0_SRC_ID_A_REG                     0x46021300: 0x4030201 
    CPSW_P0_HOST_BLKS_PRI_REG                0x46021320: 0x0 
    CPSW_PN_RESERVED_REG                     0x46022000: 0x0 
    CPSW_PN_CONTROL_REG                      0x46022004: 0x0 
    CPSW_PN_MAX_BLKS_REG                     0x46022008: 0x1004 
    CPSW_PN_BLK_CNT_REG                      0x46022010: 0x2 
    CPSW_PN_PORT_VLAN_REG                    0x46022014: 0x0 
    CPSW_PN_TX_PRI_MAP_REG                   0x46022018: 0x76543210 
    CPSW_PN_PRI_CTL_REG                      0x4602201c: 0x9000 
    CPSW_PN_RX_PRI_MAP_REG                   0x46022020: 0x76543210 
    CPSW_PN_RX_MAXLEN_REG                    0x46022024: 0x5f2 
    CPSW_PN_TX_BLKS_PRI_REG                  0x46022028: 0x1245678 
    CPSW_PN_RX_FLOW_THRESH_REG               0x4602202c: 0x40 
    CPSW_PN_IDLE2LPI_REG                     0x46022030: 0x0 
    CPSW_PN_LPI2WAKE_REG                     0x46022034: 0x0 
    CPSW_PN_EEE_STATUS_REG                   0x46022038: 0x60 
    CPSW_PN_IET_CONTROL_REG                  0x46022040: 0x0 
    CPSW_PN_IET_STATUS_REG                   0x46022044: 0x0 
    CPSW_PN_IET_VERIFY_REG                   0x46022048: 0x1312d0 
    CPSW_PN_FIFO_STATUS_REG                  0x46022050: 0xff00 
    CPSW_PN_EST_CONTROL_REG                  0x46022060: 0x0 
    CPSW_PN_TX_D_THRESH_SET_L_REG            0x46022180: 0x1f1f1f1f 
    CPSW_PN_TX_D_THRESH_SET_H_REG            0x46022184: 0x1f1f1f1f 
    CPSW_PN_TX_D_THRESH_CLR_L_REG            0x46022188: 0x0 
    CPSW_PN_TX_D_THRESH_CLR_H_REG            0x4602218c: 0x0 
    CPSW_PN_TX_G_BUF_THRESH_SET_L_REG        0x46022190: 0x1f1f1f1f 
    CPSW_PN_TX_G_BUF_THRESH_SET_H_REG        0x46022194: 0x1f1f1f1f 
    CPSW_PN_TX_G_BUF_THRESH_CLR_L_REG        0x46022198: 0x0 
    CPSW_PN_TX_G_BUF_THRESH_CLR_H_REG        0x4602219c: 0x0 
    CPSW_PN_TX_D_OFLOW_ADDVAL_L_REG          0x46022300: 0x0 
    CPSW_PN_TX_D_OFLOW_ADDVAL_H_REG          0x46022304: 0x0 
    CPSW_PN_SA_L_REG                         0x46022308: 0xe11c 
    CPSW_PN_SA_H_REG                         0x4602230c: 0x6fa95150 
    CPSW_PN_TS_CTL_REG                       0x46022310: 0x0 
    CPSW_PN_TS_SEQ_LTYPE_REG                 0x46022314: 0x1e0000 
    CPSW_PN_TS_VLAN_LTYPE_REG                0x46022318: 0x0 
    CPSW_PN_TS_CTL_LTYPE2_REG                0x4602231c: 0x0 
    CPSW_PN_TS_CTL2_REG                      0x46022320: 0x40000 
    CPSW_PN_MAC_CONTROL_REG                  0x46022330: 0xa1 
    CPSW_PN_MAC_STATUS_REG                   0x46022334: 0xf0000018 
    CPSW_PN_MAC_SOFT_RESET_REG               0x46022338: 0x0 
    CPSW_PN_MAC_BOFFTEST_REG                 0x4602233c: 0xd30000 
    CPSW_PN_MAC_RX_PAUSETIMER_REG            0x46022340: 0x0 
    CPSW_PN_MAC_EMCONTROL_REG                0x460223a0: 0x0 
    CPSW_PN_MAC_TX_GAP_REG                   0x460223a4: 0xc 
    CPSW_PN_INTERVLAN_OPX_POINTER_REG        0x460223ac: 0x0 
    CPSW_PN_INTERVLAN_OPX_A_REG              0x460223b0: 0x0 
    CPSW_PN_INTERVLAN_OPX_B_REG              0x460223b4: 0x0 
    CPSW_PN_INTERVLAN_OPX_C_REG              0x460223b8: 0x0 
    CPSW_PN_INTERVLAN_OPX_D_REG              0x460223bc: 0x0 
    CPSW_INT_REVISION                        0x46001000: 0x6690a200 
    CPSW_INT_EOI_REG                         0x46001010: 0x0 
    CPSW_INT_INTR_VECTOR_REG                 0x46001014: 0x0 
    CPSW_INT_ENABLE_REG                      0x46001100: 0x0 
    CPSW_INT_ENABLE_CLR_REG                  0x46001300: 0x0 
    CPSW_INT_STATUS_REG                      0x46001500: 0x0 
    CPSW_INT_INTR_VECTOR_REG                 0x46001a80: 0x0 
    CPSW_STAT0_RXGOODFRAMES                  0x4603a000: 0x2d20 
    CPSW_STAT0_RXBROADCASTFRAMES             0x4603a004: 0x2 
    CPSW_STAT0_RXMULTICASTFRAMES             0x4603a008: 0x1bab 
    CPSW_STAT0_RXCRCERRORS                   0x4603a010: 0x0 
    CPSW_STAT0_RXOVERSIZEDFRAMES             0x4603a018: 0x0 
    CPSW_STAT0_RXUNDERSIZEDFRAMES            0x4603a020: 0x0 
    CPSW_STAT0_RXFRAGMENTS                   0x4603a024: 0x0 
    CPSW_STAT0_ALE_DROP                      0x4603a028: 0x0 
    CPSW_STAT0_ALE_OVERRUN_DROP              0x4603a02c: 0x0 
    CPSW_STAT0_RXOCTETS                      0x4603a030: 0x2b3fae 
    CPSW_STAT0_TXGOODFRAMES                  0x4603a034: 0xa3b9 
    CPSW_STAT0_TXBROADCASTFRAMES             0x4603a038: 0x81d7 
    CPSW_STAT0_TXMULTICASTFRAMES             0x4603a03c: 0xfb0 
    CPSW_STAT0_TXOCTETS                      0x4603a064: 0x4acb5b 
    CPSW_STAT0_OCTETFRAMES64                 0x4603a068: 0x8ff1 
    CPSW_STAT0_OCTETFRAMES65T127             0x4603a06c: 0x26e6 
    CPSW_STAT0_OCTETFRAMES128T255            0x4603a070: 0x30d 
    CPSW_STAT0_OCTETFRAMES256T511            0x4603a074: 0x67a 
    CPSW_STAT0_OCTETFRAMES512T1023           0x4603a078: 0xfde 
    CPSW_STAT0_OCTETFRAMES1024TUP            0x4603a07c: 0x9d 
    CPSW_STAT0_NETOCTETS                     0x4603a080: 0x760b09 
    CPSW_STAT0_RX_BOTTOM_OF_FIFO_DROP        0x4603a084: 0x0 
    CPSW_STAT0_PORTMASK_DROP                 0x4603a088: 0x0 
    CPSW_STAT0_RX_TOP_OF_FIFO_DROP           0x4603a08c: 0x0 
    CPSW_STAT0_ALE_RATE_LIMIT_DROP           0x4603a090: 0x0 
    CPSW_STAT0_ALE_VID_INGRESS_DROP          0x4603a094: 0x0 
    CPSW_STAT0_ALE_DA_EQ_SA_DROP             0x4603a098: 0x0 
    CPSW_STAT0_ALE_BLOCK_DROP                0x4603a09c: 0x0 
    CPSW_STAT0_ALE_SECURE_DROP               0x4603a0a0: 0x0 
    CPSW_STAT0_ALE_AUTH_DROP                 0x4603a0a4: 0x0 
    CPSW_STAT0_ALE_UNKN_UNI                  0x4603a0a8: 0x0 
    CPSW_STAT0_ALE_UNKN_UNI_BCNT             0x4603a0ac: 0x0 
    CPSW_STAT0_ALE_UNKN_MLT                  0x4603a0b0: 0x0 
    CPSW_STAT0_ALE_UNKN_MLT_BCNT             0x4603a0b4: 0x0 
    CPSW_STAT0_ALE_UNKN_BRD                  0x4603a0b8: 0x0 
    CPSW_STAT0_ALE_UNKN_BRD_BCNT             0x4603a0bc: 0x0 
    CPSW_STAT0_ALE_POL_MATC,                 0x4603a0c0: 0x0 
    CPSW_STAT0_ALE_POL_MATCH_RED             0x4603a0c4: 0x0 
    CPSW_STAT0_ALE_POL_MATCH_YELLOW          0x4603a0c8: 0x0 
    CPSW_STAT0_ALE_MULT_SA_DROP              0x4603a0cc: 0x0 
    CPSW_STAT0_ALE_DUAL_VLAN_DROP            0x4603a0d0: 0x0 
    CPSW_STAT0_ALE_LEN_ERROR_DROP            0x4603a0d4: 0x0 
    CPSW_STAT0_ALE_IP_NEXT_HDR_DROP          0x4603a0d8: 0x0 
    CPSW_STAT0_ALE_IPV4_FRAG_DROP            0x4603a0dc: 0x0 
    CPSW_STAT0_IET_RX_ASSEMBLY_ERROR_REG     0x4603a140: 0x0 
    CPSW_STAT0_IET_RX_ASSEMBLY_OK_REG        0x4603a144: 0x0 
    CPSW_STAT0_IET_RX_SMD_ERROR_REG          0x4603a148: 0x0 
    CPSW_STAT0_IET_RX_FRAG_REG               0x4603a14c: 0x0 
    CPSW_STAT0_IET_TX_HOLD_REG               0x4603a150: 0x0 
    CPSW_STAT0_IET_TX_FRAG_REG               0x4603a154: 0x0 
    CPSW_STAT0_TX_MEMORY_PROTECT_ERROR       0x4603a17c: 0x0 
    CPSW_STAT1_RXGOODFRAMES                  0x4603a200: 0x3199e0 
    CPSW_STAT1_RXBROADCASTFRAMES             0x4603a204: 0x81d7 
    CPSW_STAT1_RXMULTICASTFRAMES             0x4603a208: 0x3105d2 
    CPSW_STAT1_RXPAUSEFRAMES                 0x4603a20c: 0x0 
    CPSW_STAT1_RXCRCERRORS                   0x4603a210: 0x0 
    CPSW_STAT1_RXALIGNCODEERRORS             0x4603a214: 0x0 
    CPSW_STAT1_RXOVERSIZEDFRAMES             0x4603a218: 0x0 
    CPSW_STAT1_RXJABBERFRAMES                0x4603a21c: 0x0 
    CPSW_STAT1_RXUNDERSIZEDFRAMES            0x4603a220: 0x0 
    CPSW_STAT1_RXFRAGMENTS                   0x4603a224: 0x0 
    CPSW_STAT1_ALE_DROP                      0x4603a228: 0x30f625 
    CPSW_STAT1_ALE_OVERRUN_DROP              0x4603a22c: 0x0 
    CPSW_STAT1_RXOCTETS                      0x4603a230: 0xcfa82c43 
    CPSW_STAT1_TXGOODFRAMES                  0x4603a234: 0x2d20 
    CPSW_STAT1_TXBROADCASTFRAMES             0x4603a238: 0x2 
    CPSW_STAT1_TXMULTICASTFRAMES             0x4603a23c: 0x1bab 
    CPSW_STAT1_TXPAUSEFRAMES                 0x4603a240: 0x0 
    CPSW_STAT1_TXDEFERREDFRAMES              0x4603a244: 0x0 
    CPSW_STAT1_TXCOLLISIONFRAMES             0x4603a248: 0x0 
    CPSW_STAT1_TXSINGLECOLLFRAMES            0x4603a24c: 0x0 
    CPSW_STAT1_TXMULTCOLLFRAMES              0x4603a250: 0x0 
    CPSW_STAT1_TXEXCESSIVECOLLISIONS         0x4603a254: 0x0 
    CPSW_STAT1_TXLATECOLLISIONS              0x4603a258: 0x0 
    CPSW_STAT1_RXIPGERROR                    0x4603a25c: 0x0 
    CPSW_STAT1_TXCARRIERSENSEERRORS          0x4603a260: 0x0 
    CPSW_STAT1_TXOCTETS                      0x4603a264: 0x2b3fae 
    CPSW_STAT1_OCTETFRAMES64                 0x4603a268: 0x94f4 
    CPSW_STAT1_OCTETFRAMES65T127             0x4603a26c: 0x2c16 
    CPSW_STAT1_OCTETFRAMES128T255            0x4603a270: 0x19764 
    CPSW_STAT1_OCTETFRAMES256T511            0x4603a274: 0x6cc 
    CPSW_STAT1_OCTETFRAMES512T1023           0x4603a278: 0x987d4 
    CPSW_STAT1_OCTETFRAMES1024TUP            0x4603a27c: 0x25dff3 
    CPSW_STAT1_NETOCTETS                     0x4603a280: 0xcfd3706f 
    CPSW_STAT1_RX_BOTTOM_OF_FIFO_DROP        0x4603a284: 0x0 
    CPSW_STAT1_PORTMASK_DROP                 0x4603a288: 0x30f628 
    CPSW_STAT1_RX_TOP_OF_FIFO_DROP           0x4603a28c: 0x0 
    CPSW_STAT1_ALE_RATE_LIMIT_DROP           0x4603a290: 0x0 
    CPSW_STAT1_ALE_VID_INGRESS_DROP          0x4603a294: 0x0 
    CPSW_STAT1_ALE_DA_EQ_SA_DROP             0x4603a298: 0x2 
    CPSW_STAT1_ALE_BLOCK_DROP                0x4603a29c: 0x0 
    CPSW_STAT1_ALE_SECURE_DROP               0x4603a2a0: 0x0 
    CPSW_STAT1_ALE_AUTH_DROP                 0x4603a2a4: 0x0 
    CPSW_STAT1_ALE_UNKN_UNI                  0x4603a2a8: 0x1237 
    CPSW_STAT1_ALE_UNKN_UNI_BCNT             0x4603a2ac: 0x671e5 
    CPSW_STAT1_ALE_UNKN_MLT                  0x4603a2b0: 0x3105d3 
    CPSW_STAT1_ALE_UNKN_MLT_BCNT             0x4603a2b4: 0xcf7e8344 
    CPSW_STAT1_ALE_UNKN_BRD                  0x4603a2b8: 0x81d7 
    CPSW_STAT1_ALE_UNKN_BRD_BCNT             0x4603a2bc: 0x233b98 
    CPSW_STAT1_ALE_POL_MATC                  0x4603a2c0: 0x0 
    CPSW_STAT1_ALE_POL_MATCH_RED             0x4603a2c4: 0x0 
    CPSW_STAT1_ALE_POL_MATCH_YELLOW          0x4603a2c8: 0x0 
    CPSW_STAT1_ALE_MULT_SA_DROP              0x4603a2cc: 0x0 
    CPSW_STAT1_ALE_DUAL_VLAN_DROP            0x4603a2d0: 0x0 
    CPSW_STAT1_ALE_LEN_ERROR_DROP            0x4603a2d4: 0x0 
    CPSW_STAT1_ALE_IP_NEXT_HDR_DROP          0x4603a2d8: 0x0 
    CPSW_STAT1_ALE_IPV4_FRAG_DROP            0x4603a2dc: 0x0 
    CPSW_STAT1_IET_RX_ASSEMBLY_ERROR_REG     0x4603a340: 0x0 
    CPSW_STAT1_IET_RX_ASSEMBLY_OK_REG        0x4603a344: 0x0 
    CPSW_STAT1_IET_RX_SMD_ERROR_REG          0x4603a348: 0x0 
    CPSW_STAT1_IET_RX_FRAG_REG               0x4603a34c: 0x0 
    CPSW_STAT1_IET_TX_HOLD_REG               0x4603a350: 0x0 
    CPSW_STAT1_IET_TX_FRAG_REG               0x4603a354: 0x0 
    CPSW_STAT1_TX_MEMORY_PROTECT_ERROR       0x4603a37c: 0x0 
    CPSW_ALE_MOD_VER                         0x4603e000: 0x293904 
    CPSW_ALE_STATUS                          0x4603e004: 0x140 
    CPSW_ALE_CONTROL                         0x4603e008: 0x80000004 
    CPSW_ALE_CTRL2                           0x4603e00c: 0x0 
    CPSW_ALE_PRESCALE                        0x4603e010: 0x0 
    CPSW_ALE_AGING_CTRL                      0x4603e014: 0x0 
    CPSW_ALE_NXT_HDR                         0x4603e01c: 0x0 
    CPSW_ALE_TBLCTL                          0x4603e020: 0xa 
    CPSW_ALE_TBLW2                           0x4603e034: 0x4 
    CPSW_ALE_TBLW1                           0x4603e038: 0x10000180 
    CPSW_ALE_TBLW0                           0x4603e03c: 0xc200000e 
    CPSW_ALE_UVLAN_MEMBER                    0x4603e090: 0x0 
    CPSW_ALE_UVLAN_URCAST                    0x4603e094: 0x0 
    CPSW_ALE_UVLAN_RMCAST                    0x4603e098: 0x0 
    CPSW_ALE_UVLAN_UNTAG                     0x4603e09c: 0x0 
    CPSW_ALE_STAT_DIAG                       0x4603e0b8: 0x0 
    CPSW_ALE_OAM_LB_CTRL                     0x4603e0bc: 0x0 
    CPSW_ALE_MSK_MUX0                        0x4603e0c0: 0x3 
    CPSW_ALE_EGRESSOP                        0x4603e0fc: 0x0 
    CPSW_ALE_POLICECFG0                      0x4603e100: 0x0 
    CPSW_ALE_POLICECFG1                      0x4603e104: 0x0 
    CPSW_ALE_POLICECFG2                      0x4603e108: 0x0 
    CPSW_ALE_POLICECFG3                      0x4603e10c: 0x0 
    CPSW_ALE_POLICECFG4                      0x4603e110: 0x0 
    CPSW_ALE_POLICECFG6                      0x4603e118: 0x0 
    CPSW_ALE_POLICECFG7                      0x4603e11c: 0x0 
    CPSW_ALE_POLICETBLCTL                    0x4603e120: 0x0 
    CPSW_ALE_POLICECONTROL                   0x4603e124: 0x0 
    CPSW_ALE_POLICETESTCTL                   0x4603e128: 0x0 
    CPSW_ALE_POLICEHSTAT                     0x4603e12c: 0x0 
    CPSW_ALE_THREADMAPDEF                    0x4603e134: 0x8000 
    CPSW_ALE_THREADMAPCTL                    0x4603e138: 0x0 
    CPSW_ALE_THREADMAPVAL                    0x4603e13c: 0x0 
    
    CPSW_SS_CPSW_NUSS_IDVER_REG              0xc000000: 0x6ba01901 
    CPSW_SS_SYNCE_COUNT_REG                  0xc000004: 0x0 
    CPSW_SS_SYNCE_MUX_REG                    0xc000008: 0x0 
    CPSW_SS_CONTROL_REG                      0xc00000c: 0x0 
    CPSW_SS_SGMII_NON_FIBER_MODE_REG         0xc000010: 0xff 
    CPSW_SS_SERDES_RESET_ISO_REG             0xc000014: 0x0 
    CPSW_SS_SUBSSYSTEM_STATUS_REG            0xc00001c: 0x0 
    CPSW_SS_RGMII1_STATUS_REG                0xc000030: 0x0 
    CPSW_SS_RGMII2_STATUS_REG                0xc000034: 0x0 
    CPSW_SS_RGMII3_STATUS_REG                0xc000038: 0x0 
    CPSW_SS_RGMII4_STATUS_REG                0xc00003c: 0x0 
    CPSW_SS_RGMII5_STATUS_REG                0xc000040: 0xd 
    CPSW_SS_RGMII6_STATUS_REG                0xc000044: 0x0 
    CPSW_SS_RGMII7_STATUS_REG                0xc000048: 0x0 
    CPSW_SS_RGMII8_STATUS_REG                0xc00004c: 0x0 
    CPSW_SS_QSGMII_CONTROL_REG               0xc000060: 0x0 
    CPSW_SS_QSGMII_STATUS_REG                0xc000064: 0x0 
    CPSW_SS_STATUS_XGMII_LINK_REG            0xc000074: 0x0 
    CPSW_SS_STATUS_SGMII_LINK_REG            0xc000078: 0x0 
    CPSW_MDIO_VERSION_REG                    0xc000f00: 0x70907 
    CPSW_MDIO_CONTROL_REG                    0xc000f04: 0x41000090 
    CPSW_MDIO_ALIVE_REG                      0xc000f08: 0x1 
    CPSW_MDIO_LINK_REG                       0xc000f0c: 0x1 
    CPSW_MDIO_LINK_INT_RAW_REG               0xc000f10: 0x1 
    CPSW_MDIO_LINK_INT_MASKED_REG            0xc000f14: 0x1 
    CPSW_MDIO_LINK_INT_MASK_SET_REG          0xc000f18: 0x1 
    CPSW_MDIO_LINK_INT_MASK_CLEAR_REG        0xc000f1c: 0x1 
    CPSW_MDIO_USER_INT_RAW_REG               0xc000f20: 0x1 
    CPSW_MDIO_USER_INT_MASKED_REG            0xc000f24: 0x0 
    CPSW_MDIO_USER_INT_MASK_SET_REG          0xc000f28: 0x0 
    CPSW_MDIO_USER_INT_MASK_CLEAR_REG        0xc000f2c: 0x0 
    CPSW_MDIO_MANUAL_IF_REG                  0xc000f30: 0x0 
    CPSW_MDIO_POLL_REG                       0xc000f34: 0x40000001 
    CPSW_MDIO_POLL_EN_REG                    0xc000f38: 0xffffffff 
    CPSW_MDIO_CLAUS45_REG                    0xc000f3c: 0x0 
    CPSW_MDIO_USER_ADDR0_REG                 0xc000f40: 0x0 
    CPSW_MDIO_USER_ADDR1_REG                 0xc000f44: 0x0 
    CPSW_CPTS_IDVER_REG                      0xc03d000: 0x4e8a010a 
    CPSW_CPTS_CONTROL_REG                    0xc03d004: 0xff2d 
    CPSW_CPTS_RFTCLK_SEL_REG                 0xc03d008: 0x0 
    CPSW_CPTS_TS_PUSH_REG                    0xc03d00c: 0x0 
    CPSW_CPTS_TS_LOAD_VAL_REG                0xc03d010: 0x0 
    CPSW_CPTS_TS_LOAD_EN_REG                 0xc03d014: 0x0 
    CPSW_CPTS_TS_COMP_VAL_REG                0xc03d018: 0x0 
    CPSW_CPTS_TS_COMP_LEN_REG                0xc03d01c: 0x0 
    CPSW_CPTS_INTSTAT_RAW_REG                0xc03d020: 0x0 
    CPSW_CPTS_INTSTAT_MASKED_REG             0xc03d024: 0x0 
    CPSW_CPTS_INT_ENABLE_REG                 0xc03d028: 0x1 
    CPSW_CPTS_TS_COMP_NUDGE_REG              0xc03d02c: 0x0 
    CPSW_CPTS_EVENT_POP_REG                  0xc03d030: 0x0 
    CPSW_CPTS_EVENT_0_REG                    0xc03d034: 0x388d0019 
    CPSW_CPTS_EVENT_1_REG                    0xc03d038: 0x1300000 
    CPSW_CPTS_EVENT_2_REG                    0xc03d03c: 0x0 
    CPSW_CPTS_EVENT_3_REG                    0xc03d040: 0x10c 
    CPSW_CPTS_TS_LOAD_HIGH_VAL_REG           0xc03d044: 0x0 
    CPSW_CPTS_TS_COMP_HIGH_VAL_REG           0xc03d048: 0x0 
    CPSW_CPTS_TS_ADD_VAL_REG                 0xc03d04c: 0x4 
    CPSW_CPTS_TS_PPM_LOW_VAL_REG             0xc03d050: 0x0 
    CPSW_CPTS_IDVER_REG                      0xc03d000: 0x4e8a010a 
    CPSW_CPTS_CONTROL_REG                    0xc03d004: 0xff2d 
    CPSW_CPTS_RFTCLK_SEL_REG                 0xc03d008: 0x0 
    CPSW_CPTS_TS_PUSH_REG                    0xc03d00c: 0x0 
    CPSW_CPTS_TS_LOAD_VAL_REG                0xc03d010: 0x0 
    CPSW_CPTS_TS_LOAD_EN_REG                 0xc03d014: 0x0 
    CPSW_CPTS_TS_COMP_VAL_REG                0xc03d018: 0x0 
    CPSW_CPTS_TS_COMP_LEN_REG                0xc03d01c: 0x0 
    CPSW_CPTS_INTSTAT_RAW_REG                0xc03d020: 0x0 
    CPSW_CPTS_INTSTAT_MASKED_REG             0xc03d024: 0x0 
    CPSW_CPTS_INT_ENABLE_REG                 0xc03d028: 0x1 
    CPSW_CPTS_TS_COMP_NUDGE_REG              0xc03d02c: 0x0 
    CPSW_CPTS_EVENT_POP_REG                  0xc03d030: 0x0 
    CPSW_CPTS_EVENT_0_REG                    0xc03d034: 0x388d0019 
    CPSW_CPTS_EVENT_1_REG                    0xc03d038: 0x1300000 
    CPSW_CPTS_EVENT_2_REG                    0xc03d03c: 0x0 
    CPSW_CPTS_EVENT_3_REG                    0xc03d040: 0x10c 
    CPSW_CPTS_TS_LOAD_HIGH_VAL_REG           0xc03d044: 0x0 
    CPSW_CPTS_TS_COMP_HIGH_VAL_REG           0xc03d048: 0x0 
    CPSW_CPTS_TS_ADD_VAL_REG                 0xc03d04c: 0x4 
    CPSW_CPTS_TS_PPM_LOW_VAL_REG             0xc03d050: 0x0 
    CPSW_GENF0_COMP_HIGH_REG                 0xc03d0e4: 0x0 
    CPSW_GENF0_CONTROL_REG                   0xc03d0e8: 0x2 
    CPSW_GENF0_LENGTH_REG                    0xc03d0ec: 0x3b9aca00 
    CPSW_GENF0_PPM_LOW_REG                   0xc03d0f0: 0x0 
    CPSW_GENF0_PPM_HIGH_REG                  0xc03d0f4: 0x0 
    CPSW_GENF0_NUDGE_REG                     0xc03d0f8: 0x0 
    CPSW_GENF1_COMP_LOW_REG                  0xc03d100: 0x0 
    CPSW_GENF1_COMP_HIGH_REG                 0xc03d104: 0x0 
    CPSW_GENF1_CONTROL_REG                   0xc03d108: 0x0 
    CPSW_GENF1_LENGTH_REG                    0xc03d10c: 0x0 
    CPSW_GENF1_PPM_LOW_REG                   0xc03d110: 0x0 
    CPSW_GENF1_PPM_HIGH_REG                  0xc03d114: 0x0 
    CPSW_GENF1_NUDGE_REG                     0xc03d118: 0x0 
    CPSW_GENF0_COMP_HIGH_REG                 0xc03d0e4: 0x0 
    CPSW_GENF0_CONTROL_REG                   0xc03d0e8: 0x2 
    CPSW_GENF0_LENGTH_REG                    0xc03d0ec: 0x3b9aca00 
    CPSW_GENF0_PPM_LOW_REG                   0xc03d0f0: 0x0 
    CPSW_GENF0_PPM_HIGH_REG                  0xc03d0f4: 0x0 
    CPSW_GENF0_NUDGE_REG                     0xc03d0f8: 0x0 
    CPSW_GENF1_COMP_LOW_REG                  0xc03d100: 0x0 
    CPSW_GENF1_COMP_HIGH_REG                 0xc03d104: 0x0 
    CPSW_GENF1_CONTROL_REG                   0xc03d108: 0x0 
    CPSW_GENF1_LENGTH_REG                    0xc03d10c: 0x0 
    CPSW_GENF1_PPM_LOW_REG                   0xc03d110: 0x0 
    CPSW_GENF1_PPM_HIGH_REG                  0xc03d114: 0x0 
    CPSW_GENF1_NUDGE_REG                     0xc03d118: 0x0 
    CPSW_TX_PRI3_MAXLEN_REG                  0xc02010c: 0x7e8 
    CPSW_TX_PRI4_MAXLEN_REG                  0xc020110: 0x7e8 
    CPSW_TX_PRI5_MAXLEN_REG                  0xc020114: 0x7e8 
    CPSW_TX_PRI6_MAXLEN_REG                  0xc020118: 0x7e8 
    CPSW_TX_PRI7_MAXLEN_REG                  0xc02011c: 0x7e8 
    CPSW_P0_CONTROL_REG                      0xc021004: 0x1 
    CPSW_P0_FLOW_ID_OFFSET_REG               0xc021008: 0xac 
    CPSW_P0_BLK_CNT_REG                      0xc021010: 0x2 
    CPSW_P0_PORT_VLAN_REG                    0xc021014: 0xe12c 
    CPSW_P0_TX_PRI_MAP_REG                   0xc021018: 0x76543210 
    CPSW_P0_PRI_CTL_REG                      0xc02101c: 0x0 
    CPSW_P0_RX_PRI_MAP_REG                   0xc021020: 0x76543210 
    CPSW_P0_RX_MAXLEN_REG                    0xc021024: 0x5f2 
    CPSW_P0_TX_BLKS_PRI_REG                  0xc021028: 0x1245678 
    CPSW_P0_IDLE2LPI_REG                     0xc021030: 0x0 
    CPSW_P0_LPI2WAKE_REG                     0xc021034: 0x0 
    CPSW_P0_EEE_STATUS_REG                   0xc021038: 0x60 
    CPSW_P0_FIFO_STATUS_REG                  0xc021050: 0x0 
    CPSW_P0_TX_D_THRESH_SET_L_REG            0xc021180: 0x1f1f1f1f 
    CPSW_P0_TX_D_THRESH_SET_H_REG            0xc021184: 0x1f1f1f1f 
    CPSW_P0_TX_D_THRESH_CLR_L_REG            0xc021188: 0x0 
    CPSW_P0_TX_D_THRESH_CLR_H_REG            0xc02118c: 0x0 
    CPSW_P0_TX_G_BUF_THRESH_SET_L_REG        0xc021190: 0x1f1f1f1f 
    CPSW_P0_TX_G_BUF_THRESH_SET_H_REG        0xc021194: 0x1f1f1f1f 
    CPSW_P0_TX_G_BUF_THRESH_CLR_L_REG        0xc021198: 0x0 
    CPSW_P0_TX_G_BUF_THRESH_CLR_H_REG        0xc02119c: 0x0 
    CPSW_P0_SRC_ID_A_REG                     0xc021300: 0x4030201 
    CPSW_P0_SRC_ID_B_REG                     0xc021304: 0x8070605 
    CPSW_P0_HOST_BLKS_PRI_REG                0xc021320: 0x0 
    CPSW_PN_RESERVED_REG                     0xc022000: 0x0 
    CPSW_PN_CONTROL_REG                      0xc022004: 0x0 
    CPSW_INT_REVISION                        0xc001000: 0x6690a200 
    CPSW_INT_EOI_REG                         0xc001010: 0x0 
    CPSW_INT_INTR_VECTOR_REG                 0xc001014: 0x0 
    CPSW_INT_ENABLE_REG                      0xc001100: 0x0 
    CPSW_INT_ENABLE_CLR_REG                  0xc001300: 0x0 
    CPSW_INT_STATUS_REG                      0xc001500: 0x0 
    CPSW_INT_INTR_VECTOR_REG                 0xc001a80: 0x0 
    CPSW_ALE_MOD_VER                         0xc03e000: 0x294104 
    CPSW_ALE_STATUS                          0xc03e004: 0x80000c01 
    CPSW_ALE_CONTROL                         0xc03e008: 0x800000c4 
    CPSW_ALE_CTRL2                           0xc03e00c: 0x100000 
    CPSW_ALE_PRESCALE                        0xc03e010: 0x3d090 
    CPSW_ALE_AGING_CTRL                      0xc03e014: 0x141 
    CPSW_ALE_NXT_HDR                         0xc03e01c: 0x6061106 
    CPSW_ALE_TBLCTL                          0xc03e020: 0x3ff 
    CPSW_ALE_TBLW2                           0xc03e034: 0x0 
    CPSW_ALE_TBLW1                           0xc03e038: 0x0 
    CPSW_ALE_TBLW0                           0xc03e03c: 0x0 
    CPSW_ALE_UVLAN_MEMBER                    0xc03e090: 0x0 
    CPSW_ALE_UVLAN_URCAST                    0xc03e094: 0x0 
    CPSW_ALE_UVLAN_RMCAST                    0xc03e098: 0x0 
    CPSW_ALE_UVLAN_UNTAG                     0xc03e09c: 0x0 
    CPSW_ALE_STAT_DIAG                       0xc03e0b8: 0x0 
    CPSW_ALE_OAM_LB_CTRL                     0xc03e0bc: 0x0 
    CPSW_ALE_EGRESSOP                        0xc03e0fc: 0x0 
    CPSW_ALE_POLICECFG0                      0xc03e100: 0x0 
    CPSW_ALE_POLICECFG1                      0xc03e104: 0x800b0000 
    CPSW_ALE_POLICECFG2                      0xc03e108: 0x0 
    CPSW_ALE_POLICECFG3                      0xc03e10c: 0x0 
    CPSW_ALE_POLICECFG4                      0xc03e110: 0x0 
    CPSW_ALE_POLICECFG6                      0xc03e118: 0x0 
    CPSW_ALE_POLICECFG7                      0xc03e11c: 0x0 
    CPSW_ALE_POLICETBLCTL                    0xc03e120: 0x0 
    CPSW_ALE_POLICECONTROL                   0xc03e124: 0x80000000 
    CPSW_ALE_POLICETESTCTL                   0xc03e128: 0x0 
    CPSW_ALE_POLICEHSTAT                     0xc03e12c: 0x80000000 
    CPSW_ALE_THREADMAPDEF                    0xc03e134: 0x8003 
    CPSW_ALE_THREADMAPCTL                    0xc03e138: 0x0 
    CPSW_ALE_THREADMAPVAL                    0xc03e13c: 0x8000 
    
    CPSW_SS_CPSW_NUSS_IDVER_REG              0x46000000: 0x6ba00101 
    CPSW_SS_SYNCE_COUNT_REG                  0x46000004: 0x0 
    CPSW_SS_SYNCE_MUX_REG                    0x46000008: 0x0 
    CPSW_SS_CONTROL_REG                      0x4600000c: 0x0 
    CPSW_SS_SGMII_MODE_REG                   0x46000010: 0x1 
    CPSW_SS_RGMII_STATUS_REG                 0x46000018: 0x0 
    CPSW_SS_SUBSSYSTEM_STATUS_REG            0x4600001c: 0x0 
    CPSW_MDIO_VERSION_REG                    0x46000f00: 0x70907 
    CPSW_MDIO_CONTROL_REG                    0x46000f04: 0x8100014c 
    CPSW_MDIO_ALIVE_REG                      0x46000f08: 0x8 
    CPSW_MDIO_LINK_REG                       0x46000f0c: 0x8 
    CPSW_MDIO_LINK_INT_RAW_REG               0x46000f10: 0x0 
    CPSW_MDIO_LINK_INT_MASKED_REG            0x46000f14: 0x0 
    CPSW_MDIO_LINK_INT_MASK_SET_REG          0x46000f18: 0x0 
    CPSW_MDIO_LINK_INT_MASK_CLEAR_REG        0x46000f1c: 0x0 
    CPSW_MDIO_USER_INT_RAW_REG               0x46000f20: 0x1 
    CPSW_MDIO_USER_INT_MASKED_REG            0x46000f24: 0x0 
    CPSW_MDIO_USER_INT_MASK_SET_REG          0x46000f28: 0x0 
    CPSW_MDIO_USER_INT_MASK_CLEAR_REG        0x46000f2c: 0x0 
    CPSW_MDIO_MANUAL_IF_REG                  0x46000f30: 0x1 
    CPSW_MDIO_POLL_REG                       0x46000f34: 0x0 
    CPSW_MDIO_POLL_EN_REG                    0x46000f38: 0xffffffff 
    CPSW_MDIO_CLAUS45_REG                    0x46000f3c: 0x0 
    CPSW_MDIO_USER_ADDR0_REG                 0x46000f40: 0x0 
    CPSW_MDIO_USER_ADDR1_REG                 0x46000f44: 0x0 
    CPSW_CPTS_IDVER_REG                      0x4603d000: 0x4e8a010a 
    CPSW_CPTS_CONTROL_REG                    0x4603d004: 0x21 
    CPSW_CPTS_RFTCLK_SEL_REG                 0x4603d008: 0x0 
    CPSW_CPTS_TS_PUSH_REG                    0x4603d00c: 0x0 
    CPSW_CPTS_TS_LOAD_VAL_REG                0x4603d010: 0xbe86c356 
    CPSW_CPTS_TS_LOAD_EN_REG                 0x4603d014: 0x0 
    CPSW_CPTS_TS_COMP_VAL_REG                0x4603d018: 0x0 
    CPSW_CPTS_TS_COMP_LEN_REG                0x4603d01c: 0x0 
    CPSW_CPTS_INTSTAT_RAW_REG                0x4603d020: 0x0 
    CPSW_CPTS_INTSTAT_MASKED_REG             0x4603d024: 0x0 
    CPSW_CPTS_INT_ENABLE_REG                 0x4603d028: 0x1 
    CPSW_CPTS_TS_COMP_NUDGE_REG              0x4603d02c: 0x0 
    CPSW_CPTS_EVENT_POP_REG                  0x4603d030: 0x0 
    CPSW_CPTS_EVENT_0_REG                    0x4603d034: 0x0 
    CPSW_CPTS_EVENT_1_REG                    0x4603d038: 0x0 
    CPSW_CPTS_EVENT_2_REG                    0x4603d03c: 0x0 
    CPSW_CPTS_EVENT_3_REG                    0x4603d040: 0x0 
    CPSW_CPTS_TS_LOAD_HIGH_VAL_REG           0x4603d044: 0x0 
    CPSW_CPTS_TS_COMP_HIGH_VAL_REG           0x4603d048: 0x0 
    CPSW_CPTS_TS_ADD_VAL_REG                 0x4603d04c: 0x1 
    CPSW_CPTS_TS_PPM_LOW_VAL_REG             0x4603d050: 0x0 
    CPSW_CPTS_TS_PPM_HIGH_VAL_REG            0x4603d054: 0x0 
    CPSW_CPTS_TS_NUDGE_VAL_REG               0x4603d058: 0x0 
    CPSW_GENF0_COMP_LOW_REG                  0x4603d0e0: 0x0 
    CPSW_GENF0_COMP_HIGH_REG                 0x4603d0e4: 0x0 
    CPSW_GENF0_TS_GENF_CONTROL_REG           0x4603d0e8: 0x0 
    CPSW_GENF0_LENGTH_REG                    0x4603d0ec: 0x0 
    CPSW_GENF0_PPM_LOW_REG                   0x4603d0f0: 0x0 
    CPSW_GENF0_PPM_HIGH_REG                  0x4603d0f4: 0x0 
    CPSW_GENF0_NUDGE_REG                     0x4603d0f8: 0x0 
    CPSW_GENF1_COMP_LOW_REG                  0x4603d100: 0x0 
    CPSW_GENF1_COMP_HIGH_REG                 0x4603d104: 0x0 
    CPSW_GENF1_CONTROL_REG                   0x4603d108: 0x0 
    CPSW_GENF1_LENGTH_REG                    0x4603d10c: 0x0 
    CPSW_GENF1_PPM_LOW_REG                   0x4603d110: 0x0 
    CPSW_GENF1_PPM_HIGH_REG                  0x4603d114: 0x0 
    CPSW_GENF1_NUDGE_REG                     0x4603d118: 0x0 
    CPSW_ESTF1_COMP_LOW_REG                  0x4603d200: 0x0 
    CPSW_ESTF1_COMP_HIGH_REG                 0x4603d204: 0x0 
    CPSW_ESTF1_CONTROL_REG                   0x4603d208: 0x0 
    CPSW_ESTF1_LENGTH_REG                    0x4603d20c: 0x0 
    CPSW_ESTF1_PPM_LOW_REG                   0x4603d210: 0x0 
    CPSW_ESTF1_PPM_HIGH_REG                  0x4603d214: 0x0 
    CPSW_ESTF1_NUDGE_REG                     0x4603d218: 0x0 
    CPSW_CPSW_ID_VER_REG                     0x46020000: 0x6ba80100 
    CPSW_CONTROL_REG                         0x46020004: 0x6006 
    CPSW_EM_CONTROL_REG                      0x46020010: 0x0 
    CPSW_STAT_PORT_EN_REG                    0x46020014: 0x3 
    CPSW_PTYPE_REG                           0x46020018: 0x0 
    CPSW_SOFT_IDLE_REG                       0x4602001c: 0x0 
    CPSW_THRU_RATE_REG                       0x46020020: 0x3001 
    CPSW_GAP_THRESH_REG                      0x46020024: 0xb 
    CPSW_TX_START_WDS_REG                    0x46020028: 0x8 
    CPSW_EEE_PRESCALE_REG                    0x4602002c: 0x0 
    CPSW_TX_G_OFLOW_THRESH_SET_REG           0x46020030: 0xffffffff 
    CPSW_TX_G_OFLOW_THRESH_CLR_REG           0x46020034: 0x0 
    CPSW_TX_G_BUF_THRESH_SET_L_REG           0x46020038: 0xffffffff 
    CPSW_TX_G_BUF_THRESH_SET_H_REG           0x4602003c: 0xffffffff 
    CPSW_TX_G_BUF_THRESH_CLR_L_REG           0x46020040: 0x0 
    CPSW_TX_G_BUF_THRESH_CLR_H_REG           0x46020044: 0x0 
    CPSW_VLAN_LTYPE_REG                      0x46020050: 0x88a88100 
    CPSW_EST_TS_DOMAIN_REG                   0x46020054: 0x0 
    CPSW_TX_PRI0_MAXLEN_REG                  0x46020100: 0x7e8 
    CPSW_TX_PRI1_MAXLEN_REG                  0x46020104: 0x7e8 
    CPSW_TX_PRI2_MAXLEN_REG                  0x46020108: 0x7e8 
    CPSW_TX_PRI3_MAXLEN_REG                  0x4602010c: 0x7e8 
    CPSW_TX_PRI4_MAXLEN_REG                  0x46020110: 0x7e8 
    CPSW_TX_PRI5_MAXLEN_REG                  0x46020114: 0x7e8 
    CPSW_TX_PRI6_MAXLEN_REG                  0x46020118: 0x7e8 
    CPSW_TX_PRI7_MAXLEN_REG                  0x4602011c: 0x7e8 
    CPSW_P0_CONTROL_REG                      0x46021004: 0x1 
    CPSW_P0_FLOW_ID_OFFSET_REG               0x46021008: 0x30 
    CPSW_P0_BLK_CNT_REG                      0x46021010: 0x2 
    CPSW_P0_PORT_VLAN_REG                    0x46021014: 0x0 
    CPSW_P0_TX_PRI_MAP_REG                   0x46021018: 0x76543210 
    CPSW_P0_PRI_CTL_REG                      0x4602101c: 0x0 
    CPSW_P0_RX_PRI_MAP_REG                   0x46021020: 0x76543210 
    CPSW_P0_RX_MAXLEN_REG                    0x46021024: 0x5f2 
    CPSW_P0_TX_BLKS_PRI_REG                  0x46021028: 0x1245678 
    CPSW_P0_IDLE2LPI_REG                     0x46021030: 0x0 
    CPSW_P0_LPI2WAKE_REG                     0x46021034: 0x0 
    CPSW_P0_EEE_STATUS_REG                   0x46021038: 0x60 
    CPSW_P0_RX_PKTS_PRI_REG                  0x4602103c: 0x0 
    CPSW_P0_RX_GAP_REG                       0x4602104c: 0x1000000 
    CPSW_P0_FIFO_STATUS_REG                  0x46021050: 0x0 
    CPSW_P0_TX_D_THRESH_SET_L_REG            0x46021180: 0x1f1f1f1f 
    CPSW_P0_TX_D_THRESH_SET_H_REG            0x46021184: 0x1f1f1f1f 
    CPSW_P0_TX_D_THRESH_CLR_L_REG            0x46021188: 0x0 
    CPSW_P0_TX_D_THRESH_CLR_H_REG            0x4602118c: 0x0 
    CPSW_P0_TX_G_BUF_THRESH_SET_L_REG        0x46021190: 0x1f1f1f1f 
    CPSW_P0_TX_G_BUF_THRESH_SET_H_REG        0x46021194: 0x1f1f1f1f 
    CPSW_P0_TX_G_BUF_THRESH_CLR_L_REG        0x46021198: 0x0 
    CPSW_P0_TX_G_BUF_THRESH_CLR_H_REG        0x4602119c: 0x0 
    CPSW_P0_SRC_ID_A_REG                     0x46021300: 0x4030201 
    CPSW_P0_HOST_BLKS_PRI_REG                0x46021320: 0x0 
    CPSW_PN_RESERVED_REG                     0x46022000: 0x0 
    CPSW_PN_CONTROL_REG                      0x46022004: 0x0 
    CPSW_PN_MAX_BLKS_REG                     0x46022008: 0x1004 
    CPSW_PN_BLK_CNT_REG                      0x46022010: 0x2 
    CPSW_PN_PORT_VLAN_REG                    0x46022014: 0x0 
    CPSW_PN_TX_PRI_MAP_REG                   0x46022018: 0x76543210 
    CPSW_PN_PRI_CTL_REG                      0x4602201c: 0x9000 
    CPSW_PN_RX_PRI_MAP_REG                   0x46022020: 0x76543210 
    CPSW_PN_RX_MAXLEN_REG                    0x46022024: 0x5f2 
    CPSW_PN_TX_BLKS_PRI_REG                  0x46022028: 0x1245678 
    CPSW_PN_RX_FLOW_THRESH_REG               0x4602202c: 0x40 
    CPSW_PN_IDLE2LPI_REG                     0x46022030: 0x0 
    CPSW_PN_LPI2WAKE_REG                     0x46022034: 0x0 
    CPSW_PN_EEE_STATUS_REG                   0x46022038: 0x60 
    CPSW_PN_IET_CONTROL_REG                  0x46022040: 0x0 
    CPSW_PN_IET_STATUS_REG                   0x46022044: 0x0 
    CPSW_PN_IET_VERIFY_REG                   0x46022048: 0x1312d0 
    CPSW_PN_FIFO_STATUS_REG                  0x46022050: 0xff00 
    CPSW_PN_EST_CONTROL_REG                  0x46022060: 0x0 
    CPSW_PN_TX_D_THRESH_SET_L_REG            0x46022180: 0x1f1f1f1f 
    CPSW_PN_TX_D_THRESH_SET_H_REG            0x46022184: 0x1f1f1f1f 
    CPSW_PN_TX_D_THRESH_CLR_L_REG            0x46022188: 0x0 
    CPSW_PN_TX_D_THRESH_CLR_H_REG            0x4602218c: 0x0 
    CPSW_PN_TX_G_BUF_THRESH_SET_L_REG        0x46022190: 0x1f1f1f1f 
    CPSW_PN_TX_G_BUF_THRESH_SET_H_REG        0x46022194: 0x1f1f1f1f 
    CPSW_PN_TX_G_BUF_THRESH_CLR_L_REG        0x46022198: 0x0 
    CPSW_PN_TX_G_BUF_THRESH_CLR_H_REG        0x4602219c: 0x0 
    CPSW_PN_TX_D_OFLOW_ADDVAL_L_REG          0x46022300: 0x0 
    CPSW_PN_TX_D_OFLOW_ADDVAL_H_REG          0x46022304: 0x0 
    CPSW_PN_SA_L_REG                         0x46022308: 0xe11c 
    CPSW_PN_SA_H_REG                         0x4602230c: 0x6fa95152 
    CPSW_PN_TS_CTL_REG                       0x46022310: 0x0 
    CPSW_PN_TS_SEQ_LTYPE_REG                 0x46022314: 0x1e0000 
    CPSW_PN_TS_VLAN_LTYPE_REG                0x46022318: 0x0 
    CPSW_PN_TS_CTL_LTYPE2_REG                0x4602231c: 0x0 
    CPSW_PN_TS_CTL2_REG                      0x46022320: 0x40000 
    CPSW_PN_MAC_CONTROL_REG                  0x46022330: 0xa1 
    CPSW_PN_MAC_STATUS_REG                   0x46022334: 0xf0000018 
    CPSW_PN_MAC_SOFT_RESET_REG               0x46022338: 0x0 
    CPSW_PN_MAC_BOFFTEST_REG                 0x4602233c: 0x32a0000 
    CPSW_PN_MAC_RX_PAUSETIMER_REG            0x46022340: 0x0 
    CPSW_PN_MAC_EMCONTROL_REG                0x460223a0: 0x0 
    CPSW_PN_MAC_TX_GAP_REG                   0x460223a4: 0xc 
    CPSW_PN_INTERVLAN_OPX_POINTER_REG        0x460223ac: 0x0 
    CPSW_PN_INTERVLAN_OPX_A_REG              0x460223b0: 0x0 
    CPSW_PN_INTERVLAN_OPX_B_REG              0x460223b4: 0x0 
    CPSW_PN_INTERVLAN_OPX_C_REG              0x460223b8: 0x0 
    CPSW_PN_INTERVLAN_OPX_D_REG              0x460223bc: 0x0 
    CPSW_INT_REVISION                        0x46001000: 0x6690a200 
    CPSW_INT_EOI_REG                         0x46001010: 0x0 
    CPSW_INT_INTR_VECTOR_REG                 0x46001014: 0x0 
    CPSW_INT_ENABLE_REG                      0x46001100: 0x0 
    CPSW_INT_ENABLE_CLR_REG                  0x46001300: 0x0 
    CPSW_INT_STATUS_REG                      0x46001500: 0x0 
    CPSW_INT_INTR_VECTOR_REG                 0x46001a80: 0x0 
    CPSW_STAT0_RXGOODFRAMES                  0x4603a000: 0x1140 
    CPSW_STAT0_RXBROADCASTFRAMES             0x4603a004: 0x0 
    CPSW_STAT0_RXMULTICASTFRAMES             0x4603a008: 0x8a1 
    CPSW_STAT0_RXCRCERRORS                   0x4603a010: 0x0 
    CPSW_STAT0_RXOVERSIZEDFRAMES             0x4603a018: 0x0 
    CPSW_STAT0_RXUNDERSIZEDFRAMES            0x4603a020: 0x0 
    CPSW_STAT0_RXFRAGMENTS                   0x4603a024: 0x0 
    CPSW_STAT0_ALE_DROP                      0x4603a028: 0x0 
    CPSW_STAT0_ALE_OVERRUN_DROP              0x4603a02c: 0x0 
    CPSW_STAT0_RXOCTETS                      0x4603a030: 0x1d3326 
    CPSW_STAT0_TXGOODFRAMES                  0x4603a034: 0x7850 
    CPSW_STAT0_TXBROADCASTFRAMES             0x4603a038: 0x61ae 
    CPSW_STAT0_TXMULTICASTFRAMES             0x4603a03c: 0xc58 
    CPSW_STAT0_TXOCTETS                      0x4603a064: 0x36b526 
    CPSW_STAT0_OCTETFRAMES64                 0x4603a068: 0x62fb 
    CPSW_STAT0_OCTETFRAMES65T127             0x4603a06c: 0x11de 
    CPSW_STAT0_OCTETFRAMES128T255            0x4603a070: 0x2e1 
    CPSW_STAT0_OCTETFRAMES256T511            0x4603a074: 0x522 
    CPSW_STAT0_OCTETFRAMES512T1023           0x4603a078: 0xc90 
    CPSW_STAT0_OCTETFRAMES1024TUP            0x4603a07c: 0x24 
    CPSW_STAT0_NETOCTETS                     0x4603a080: 0x53e84c 
    CPSW_STAT0_RX_BOTTOM_OF_FIFO_DROP        0x4603a084: 0x0 
    CPSW_STAT0_PORTMASK_DROP                 0x4603a088: 0x0 
    CPSW_STAT0_RX_TOP_OF_FIFO_DROP           0x4603a08c: 0x0 
    CPSW_STAT0_ALE_RATE_LIMIT_DROP           0x4603a090: 0x0 
    CPSW_STAT0_ALE_VID_INGRESS_DROP          0x4603a094: 0x0 
    CPSW_STAT0_ALE_DA_EQ_SA_DROP             0x4603a098: 0x0 
    CPSW_STAT0_ALE_BLOCK_DROP                0x4603a09c: 0x0 
    CPSW_STAT0_ALE_SECURE_DROP               0x4603a0a0: 0x0 
    CPSW_STAT0_ALE_AUTH_DROP                 0x4603a0a4: 0x0 
    CPSW_STAT0_ALE_UNKN_UNI                  0x4603a0a8: 0x0 
    CPSW_STAT0_ALE_UNKN_UNI_BCNT             0x4603a0ac: 0x0 
    CPSW_STAT0_ALE_UNKN_MLT                  0x4603a0b0: 0x0 
    CPSW_STAT0_ALE_UNKN_MLT_BCNT             0x4603a0b4: 0x0 
    CPSW_STAT0_ALE_UNKN_BRD                  0x4603a0b8: 0x0 
    CPSW_STAT0_ALE_UNKN_BRD_BCNT             0x4603a0bc: 0x0 
    CPSW_STAT0_ALE_POL_MATC,                 0x4603a0c0: 0x0 
    CPSW_STAT0_ALE_POL_MATCH_RED             0x4603a0c4: 0x0 
    CPSW_STAT0_ALE_POL_MATCH_YELLOW          0x4603a0c8: 0x0 
    CPSW_STAT0_ALE_MULT_SA_DROP              0x4603a0cc: 0x0 
    CPSW_STAT0_ALE_DUAL_VLAN_DROP            0x4603a0d0: 0x0 
    CPSW_STAT0_ALE_LEN_ERROR_DROP            0x4603a0d4: 0x0 
    CPSW_STAT0_ALE_IP_NEXT_HDR_DROP          0x4603a0d8: 0x0 
    CPSW_STAT0_ALE_IPV4_FRAG_DROP            0x4603a0dc: 0x0 
    CPSW_STAT0_IET_RX_ASSEMBLY_ERROR_REG     0x4603a140: 0x0 
    CPSW_STAT0_IET_RX_ASSEMBLY_OK_REG        0x4603a144: 0x0 
    CPSW_STAT0_IET_RX_SMD_ERROR_REG          0x4603a148: 0x0 
    CPSW_STAT0_IET_RX_FRAG_REG               0x4603a14c: 0x0 
    CPSW_STAT0_IET_TX_HOLD_REG               0x4603a150: 0x0 
    CPSW_STAT0_IET_TX_FRAG_REG               0x4603a154: 0x0 
    CPSW_STAT0_TX_MEMORY_PROTECT_ERROR       0x4603a17c: 0x0 
    CPSW_STAT1_RXGOODFRAMES                  0x4603a200: 0x25b898 
    CPSW_STAT1_RXBROADCASTFRAMES             0x4603a204: 0x61ae 
    CPSW_STAT1_RXMULTICASTFRAMES             0x4603a208: 0x254c9b 
    CPSW_STAT1_RXPAUSEFRAMES                 0x4603a20c: 0x0 
    CPSW_STAT1_RXCRCERRORS                   0x4603a210: 0x0 
    CPSW_STAT1_RXALIGNCODEERRORS             0x4603a214: 0x0 
    CPSW_STAT1_RXOVERSIZEDFRAMES             0x4603a218: 0x0 
    CPSW_STAT1_RXJABBERFRAMES                0x4603a21c: 0x0 
    CPSW_STAT1_RXUNDERSIZEDFRAMES            0x4603a220: 0x0 
    CPSW_STAT1_RXFRAGMENTS                   0x4603a224: 0x0 
    CPSW_STAT1_ALE_DROP                      0x4603a228: 0x254046 
    CPSW_STAT1_ALE_OVERRUN_DROP              0x4603a22c: 0x0 
    CPSW_STAT1_RXOCTETS                      0x4603a230: 0x9dc5f716 
    CPSW_STAT1_TXGOODFRAMES                  0x4603a234: 0x1140 
    CPSW_STAT1_TXBROADCASTFRAMES             0x4603a238: 0x0 
    CPSW_STAT1_TXMULTICASTFRAMES             0x4603a23c: 0x8a1 
    CPSW_STAT1_TXPAUSEFRAMES                 0x4603a240: 0x0 
    CPSW_STAT1_TXDEFERREDFRAMES              0x4603a244: 0x0 
    CPSW_STAT1_TXCOLLISIONFRAMES             0x4603a248: 0x0 
    CPSW_STAT1_TXSINGLECOLLFRAMES            0x4603a24c: 0x0 
    CPSW_STAT1_TXMULTCOLLFRAMES              0x4603a250: 0x0 
    CPSW_STAT1_TXEXCESSIVECOLLISIONS         0x4603a254: 0x0 
    CPSW_STAT1_TXLATECOLLISIONS              0x4603a258: 0x0 
    CPSW_STAT1_RXIPGERROR                    0x4603a25c: 0x0 
    CPSW_STAT1_TXCARRIERSENSEERRORS          0x4603a260: 0x0 
    CPSW_STAT1_TXOCTETS                      0x4603a264: 0x1d3326 
    CPSW_STAT1_OCTETFRAMES64                 0x4603a268: 0x6a84 
    CPSW_STAT1_OCTETFRAMES65T127             0x4603a26c: 0x1f9d 
    CPSW_STAT1_OCTETFRAMES128T255            0x4603a270: 0x13614 
    CPSW_STAT1_OCTETFRAMES256T511            0x4603a274: 0x571 
    CPSW_STAT1_OCTETFRAMES512T1023           0x4603a278: 0x73e2e 
    CPSW_STAT1_OCTETFRAMES1024TUP            0x4603a27c: 0x1cc605 
    CPSW_STAT1_NETOCTETS                     0x4603a280: 0x9de32eba 
    CPSW_STAT1_RX_BOTTOM_OF_FIFO_DROP        0x4603a284: 0x0 
    CPSW_STAT1_PORTMASK_DROP                 0x4603a288: 0x254049 
    CPSW_STAT1_RX_TOP_OF_FIFO_DROP           0x4603a28c: 0x0 
    CPSW_STAT1_ALE_RATE_LIMIT_DROP           0x4603a290: 0x0 
    CPSW_STAT1_ALE_VID_INGRESS_DROP          0x4603a294: 0x0 
    CPSW_STAT1_ALE_DA_EQ_SA_DROP             0x4603a298: 0x2 
    CPSW_STAT1_ALE_BLOCK_DROP                0x4603a29c: 0x0 
    CPSW_STAT1_ALE_SECURE_DROP               0x4603a2a0: 0x0 
    CPSW_STAT1_ALE_AUTH_DROP                 0x4603a2a4: 0x0 
    CPSW_STAT1_ALE_UNKN_UNI                  0x4603a2a8: 0xa4f 
    CPSW_STAT1_ALE_UNKN_UNI_BCNT             0x4603a2ac: 0x47af8 
    CPSW_STAT1_ALE_UNKN_MLT                  0x4603a2b0: 0x254c9c 
    CPSW_STAT1_ALE_UNKN_MLT_BCNT             0x4603a2b4: 0x9da6e3ce 
    CPSW_STAT1_ALE_UNKN_BRD                  0x4603a2b8: 0x61ae 
    CPSW_STAT1_ALE_UNKN_BRD_BCNT             0x4603a2bc: 0x1a9cce 
    CPSW_STAT1_ALE_POL_MATC                  0x4603a2c0: 0x0 
    CPSW_STAT1_ALE_POL_MATCH_RED             0x4603a2c4: 0x0 
    CPSW_STAT1_ALE_POL_MATCH_YELLOW          0x4603a2c8: 0x0 
    CPSW_STAT1_ALE_MULT_SA_DROP              0x4603a2cc: 0x0 
    CPSW_STAT1_ALE_DUAL_VLAN_DROP            0x4603a2d0: 0x0 
    CPSW_STAT1_ALE_LEN_ERROR_DROP            0x4603a2d4: 0x0 
    CPSW_STAT1_ALE_IP_NEXT_HDR_DROP          0x4603a2d8: 0x0 
    CPSW_STAT1_ALE_IPV4_FRAG_DROP            0x4603a2dc: 0x0 
    CPSW_STAT1_IET_RX_ASSEMBLY_ERROR_REG     0x4603a340: 0x0 
    CPSW_STAT1_IET_RX_ASSEMBLY_OK_REG        0x4603a344: 0x0 
    CPSW_STAT1_IET_RX_SMD_ERROR_REG          0x4603a348: 0x0 
    CPSW_STAT1_IET_RX_FRAG_REG               0x4603a34c: 0x0 
    CPSW_STAT1_IET_TX_HOLD_REG               0x4603a350: 0x0 
    CPSW_STAT1_IET_TX_FRAG_REG               0x4603a354: 0x0 
    CPSW_STAT1_TX_MEMORY_PROTECT_ERROR       0x4603a37c: 0x0 
    CPSW_ALE_MOD_VER                         0x4603e000: 0x293904 
    CPSW_ALE_STATUS                          0x4603e004: 0x140 
    CPSW_ALE_CONTROL                         0x4603e008: 0x80000004 
    CPSW_ALE_CTRL2                           0x4603e00c: 0x0 
    CPSW_ALE_PRESCALE                        0x4603e010: 0x0 
    CPSW_ALE_AGING_CTRL                      0x4603e014: 0x0 
    CPSW_ALE_NXT_HDR                         0x4603e01c: 0x0 
    CPSW_ALE_TBLCTL                          0x4603e020: 0x8 
    CPSW_ALE_TBLW2                           0x4603e034: 0x4 
    CPSW_ALE_TBLW1                           0x4603e038: 0x10003333 
    CPSW_ALE_TBLW0                           0x4603e03c: 0xfb 
    CPSW_ALE_UVLAN_MEMBER                    0x4603e090: 0x0 
    CPSW_ALE_UVLAN_URCAST                    0x4603e094: 0x0 
    CPSW_ALE_UVLAN_RMCAST                    0x4603e098: 0x0 
    CPSW_ALE_UVLAN_UNTAG                     0x4603e09c: 0x0 
    CPSW_ALE_STAT_DIAG                       0x4603e0b8: 0x0 
    CPSW_ALE_OAM_LB_CTRL                     0x4603e0bc: 0x0 
    CPSW_ALE_MSK_MUX0                        0x4603e0c0: 0x3 
    CPSW_ALE_EGRESSOP                        0x4603e0fc: 0x0 
    CPSW_ALE_POLICECFG0                      0x4603e100: 0x0 
    CPSW_ALE_POLICECFG1                      0x4603e104: 0x0 
    CPSW_ALE_POLICECFG2                      0x4603e108: 0x0 
    CPSW_ALE_POLICECFG3                      0x4603e10c: 0x0 
    CPSW_ALE_POLICECFG4                      0x4603e110: 0x0 
    CPSW_ALE_POLICECFG6                      0x4603e118: 0x0 
    CPSW_ALE_POLICECFG7                      0x4603e11c: 0x0 
    CPSW_ALE_POLICETBLCTL                    0x4603e120: 0x0 
    CPSW_ALE_POLICECONTROL                   0x4603e124: 0x0 
    CPSW_ALE_POLICETESTCTL                   0x4603e128: 0x0 
    CPSW_ALE_POLICEHSTAT                     0x4603e12c: 0x0 
    CPSW_ALE_THREADMAPDEF                    0x4603e134: 0x8000 
    CPSW_ALE_THREADMAPCTL                    0x4603e138: 0x0 
    CPSW_ALE_THREADMAPVAL                    0x4603e13c: 0x0 
    
    CPSW_SS_CPSW_NUSS_IDVER_REG              0xc000000: 0x6ba01901 
    CPSW_SS_SYNCE_COUNT_REG                  0xc000004: 0x0 
    CPSW_SS_SYNCE_MUX_REG                    0xc000008: 0x0 
    CPSW_SS_CONTROL_REG                      0xc00000c: 0x0 
    CPSW_SS_SGMII_NON_FIBER_MODE_REG         0xc000010: 0xff 
    CPSW_SS_SERDES_RESET_ISO_REG             0xc000014: 0x0 
    CPSW_SS_SUBSSYSTEM_STATUS_REG            0xc00001c: 0x0 
    CPSW_SS_RGMII1_STATUS_REG                0xc000030: 0x0 
    CPSW_SS_RGMII2_STATUS_REG                0xc000034: 0x0 
    CPSW_SS_RGMII3_STATUS_REG                0xc000038: 0x0 
    CPSW_SS_RGMII4_STATUS_REG                0xc00003c: 0x0 
    CPSW_SS_RGMII5_STATUS_REG                0xc000040: 0xd 
    CPSW_SS_RGMII6_STATUS_REG                0xc000044: 0x0 
    CPSW_SS_RGMII7_STATUS_REG                0xc000048: 0x0 
    CPSW_SS_RGMII8_STATUS_REG                0xc00004c: 0x0 
    CPSW_SS_QSGMII_CONTROL_REG               0xc000060: 0x0 
    CPSW_SS_QSGMII_STATUS_REG                0xc000064: 0x1 
    CPSW_SS_STATUS_XGMII_LINK_REG            0xc000074: 0x0 
    CPSW_SS_STATUS_SGMII_LINK_REG            0xc000078: 0x0 
    CPSW_MDIO_VERSION_REG                    0xc000f00: 0x70907 
    CPSW_MDIO_CONTROL_REG                    0xc000f04: 0x41000090 
    CPSW_MDIO_ALIVE_REG                      0xc000f08: 0x1 
    CPSW_MDIO_LINK_REG                       0xc000f0c: 0x1 
    CPSW_MDIO_LINK_INT_RAW_REG               0xc000f10: 0x1 
    CPSW_MDIO_LINK_INT_MASKED_REG            0xc000f14: 0x1 
    CPSW_MDIO_LINK_INT_MASK_SET_REG          0xc000f18: 0x1 
    CPSW_MDIO_LINK_INT_MASK_CLEAR_REG        0xc000f1c: 0x1 
    CPSW_MDIO_USER_INT_RAW_REG               0xc000f20: 0x1 
    CPSW_MDIO_USER_INT_MASKED_REG            0xc000f24: 0x0 
    CPSW_MDIO_USER_INT_MASK_SET_REG          0xc000f28: 0x0 
    CPSW_MDIO_USER_INT_MASK_CLEAR_REG        0xc000f2c: 0x0 
    CPSW_MDIO_MANUAL_IF_REG                  0xc000f30: 0x0 
    CPSW_MDIO_POLL_REG                       0xc000f34: 0x40000001 
    CPSW_MDIO_POLL_EN_REG                    0xc000f38: 0xffffffff 
    CPSW_MDIO_CLAUS45_REG                    0xc000f3c: 0x0 
    CPSW_MDIO_USER_ADDR0_REG                 0xc000f40: 0x0 
    CPSW_MDIO_USER_ADDR1_REG                 0xc000f44: 0x0 
    CPSW_CPTS_IDVER_REG                      0xc03d000: 0x4e8a010a 
    CPSW_CPTS_CONTROL_REG                    0xc03d004: 0xff2d 
    CPSW_CPTS_RFTCLK_SEL_REG                 0xc03d008: 0x0 
    CPSW_CPTS_TS_PUSH_REG                    0xc03d00c: 0x0 
    CPSW_CPTS_TS_LOAD_VAL_REG                0xc03d010: 0x0 
    CPSW_CPTS_TS_LOAD_EN_REG                 0xc03d014: 0x0 
    CPSW_CPTS_TS_COMP_VAL_REG                0xc03d018: 0x0 
    CPSW_CPTS_TS_COMP_LEN_REG                0xc03d01c: 0x0 
    CPSW_CPTS_INTSTAT_RAW_REG                0xc03d020: 0x0 
    CPSW_CPTS_INTSTAT_MASKED_REG             0xc03d024: 0x0 
    CPSW_CPTS_INT_ENABLE_REG                 0xc03d028: 0x1 
    CPSW_CPTS_TS_COMP_NUDGE_REG              0xc03d02c: 0x0 
    CPSW_CPTS_EVENT_POP_REG                  0xc03d030: 0x0 
    CPSW_CPTS_EVENT_0_REG                    0xc03d034: 0x0 
    CPSW_CPTS_EVENT_1_REG                    0xc03d038: 0x0 
    CPSW_CPTS_EVENT_2_REG                    0xc03d03c: 0x0 
    CPSW_CPTS_EVENT_3_REG                    0xc03d040: 0x0 
    CPSW_CPTS_TS_LOAD_HIGH_VAL_REG           0xc03d044: 0x0 
    CPSW_CPTS_TS_COMP_HIGH_VAL_REG           0xc03d048: 0x0 
    CPSW_CPTS_TS_ADD_VAL_REG                 0xc03d04c: 0x4 
    CPSW_CPTS_TS_PPM_LOW_VAL_REG             0xc03d050: 0x0 
    CPSW_CPTS_IDVER_REG                      0xc03d000: 0x4e8a010a 
    CPSW_CPTS_CONTROL_REG                    0xc03d004: 0xff2d 
    CPSW_CPTS_RFTCLK_SEL_REG                 0xc03d008: 0x0 
    CPSW_CPTS_TS_PUSH_REG                    0xc03d00c: 0x0 
    CPSW_CPTS_TS_LOAD_VAL_REG                0xc03d010: 0x0 
    CPSW_CPTS_TS_LOAD_EN_REG                 0xc03d014: 0x0 
    CPSW_CPTS_TS_COMP_VAL_REG                0xc03d018: 0x0 
    CPSW_CPTS_TS_COMP_LEN_REG                0xc03d01c: 0x0 
    CPSW_CPTS_INTSTAT_RAW_REG                0xc03d020: 0x0 
    CPSW_CPTS_INTSTAT_MASKED_REG             0xc03d024: 0x0 
    CPSW_CPTS_INT_ENABLE_REG                 0xc03d028: 0x1 
    CPSW_CPTS_TS_COMP_NUDGE_REG              0xc03d02c: 0x0 
    CPSW_CPTS_EVENT_POP_REG                  0xc03d030: 0x0 
    CPSW_CPTS_EVENT_0_REG                    0xc03d034: 0x0 
    CPSW_CPTS_EVENT_1_REG                    0xc03d038: 0x0 
    CPSW_CPTS_EVENT_2_REG                    0xc03d03c: 0x0 
    CPSW_CPTS_EVENT_3_REG                    0xc03d040: 0x0 
    CPSW_CPTS_TS_LOAD_HIGH_VAL_REG           0xc03d044: 0x0 
    CPSW_CPTS_TS_COMP_HIGH_VAL_REG           0xc03d048: 0x0 
    CPSW_CPTS_TS_ADD_VAL_REG                 0xc03d04c: 0x4 
    CPSW_CPTS_TS_PPM_LOW_VAL_REG             0xc03d050: 0x0 
    CPSW_GENF0_COMP_HIGH_REG                 0xc03d0e4: 0x0 
    CPSW_GENF0_CONTROL_REG                   0xc03d0e8: 0x0 
    CPSW_GENF0_LENGTH_REG                    0xc03d0ec: 0x0 
    CPSW_GENF0_PPM_LOW_REG                   0xc03d0f0: 0x0 
    CPSW_GENF0_PPM_HIGH_REG                  0xc03d0f4: 0x0 
    CPSW_GENF0_NUDGE_REG                     0xc03d0f8: 0x0 
    CPSW_GENF1_COMP_LOW_REG                  0xc03d100: 0x0 
    CPSW_GENF1_COMP_HIGH_REG                 0xc03d104: 0x0 
    CPSW_GENF1_CONTROL_REG                   0xc03d108: 0x0 
    CPSW_GENF1_LENGTH_REG                    0xc03d10c: 0x0 
    CPSW_GENF1_PPM_LOW_REG                   0xc03d110: 0x0 
    CPSW_GENF1_PPM_HIGH_REG                  0xc03d114: 0x0 
    CPSW_GENF1_NUDGE_REG                     0xc03d118: 0x0 
    CPSW_GENF0_COMP_HIGH_REG                 0xc03d0e4: 0x0 
    CPSW_GENF0_CONTROL_REG                   0xc03d0e8: 0x0 
    CPSW_GENF0_LENGTH_REG                    0xc03d0ec: 0x0 
    CPSW_GENF0_PPM_LOW_REG                   0xc03d0f0: 0x0 
    CPSW_GENF0_PPM_HIGH_REG                  0xc03d0f4: 0x0 
    CPSW_GENF0_NUDGE_REG                     0xc03d0f8: 0x0 
    CPSW_GENF1_COMP_LOW_REG                  0xc03d100: 0x0 
    CPSW_GENF1_COMP_HIGH_REG                 0xc03d104: 0x0 
    CPSW_GENF1_CONTROL_REG                   0xc03d108: 0x0 
    CPSW_GENF1_LENGTH_REG                    0xc03d10c: 0x0 
    CPSW_GENF1_PPM_LOW_REG                   0xc03d110: 0x0 
    CPSW_GENF1_PPM_HIGH_REG                  0xc03d114: 0x0 
    CPSW_GENF1_NUDGE_REG                     0xc03d118: 0x0 
    CPSW_TX_PRI3_MAXLEN_REG                  0xc02010c: 0x7e8 
    CPSW_TX_PRI4_MAXLEN_REG                  0xc020110: 0x7e8 
    CPSW_TX_PRI5_MAXLEN_REG                  0xc020114: 0x7e8 
    CPSW_TX_PRI6_MAXLEN_REG                  0xc020118: 0x7e8 
    CPSW_TX_PRI7_MAXLEN_REG                  0xc02011c: 0x7e8 
    CPSW_P0_CONTROL_REG                      0xc021004: 0x1 
    CPSW_P0_FLOW_ID_OFFSET_REG               0xc021008: 0xac 
    CPSW_P0_BLK_CNT_REG                      0xc021010: 0x2 
    CPSW_P0_PORT_VLAN_REG                    0xc021014: 0xe12c 
    CPSW_P0_TX_PRI_MAP_REG                   0xc021018: 0x76543210 
    CPSW_P0_PRI_CTL_REG                      0xc02101c: 0x0 
    CPSW_P0_RX_PRI_MAP_REG                   0xc021020: 0x76543210 
    CPSW_P0_RX_MAXLEN_REG                    0xc021024: 0x5f2 
    CPSW_P0_TX_BLKS_PRI_REG                  0xc021028: 0x1245678 
    CPSW_P0_IDLE2LPI_REG                     0xc021030: 0x0 
    CPSW_P0_LPI2WAKE_REG                     0xc021034: 0x0 
    CPSW_P0_EEE_STATUS_REG                   0xc021038: 0x60 
    CPSW_P0_FIFO_STATUS_REG                  0xc021050: 0x0 
    CPSW_P0_TX_D_THRESH_SET_L_REG            0xc021180: 0x1f1f1f1f 
    CPSW_P0_TX_D_THRESH_SET_H_REG            0xc021184: 0x1f1f1f1f 
    CPSW_P0_TX_D_THRESH_CLR_L_REG            0xc021188: 0x0 
    CPSW_P0_TX_D_THRESH_CLR_H_REG            0xc02118c: 0x0 
    CPSW_P0_TX_G_BUF_THRESH_SET_L_REG        0xc021190: 0x1f1f1f1f 
    CPSW_P0_TX_G_BUF_THRESH_SET_H_REG        0xc021194: 0x1f1f1f1f 
    CPSW_P0_TX_G_BUF_THRESH_CLR_L_REG        0xc021198: 0x0 
    CPSW_P0_TX_G_BUF_THRESH_CLR_H_REG        0xc02119c: 0x0 
    CPSW_P0_SRC_ID_A_REG                     0xc021300: 0x4030201 
    CPSW_P0_SRC_ID_B_REG                     0xc021304: 0x8070605 
    CPSW_P0_HOST_BLKS_PRI_REG                0xc021320: 0x0 
    CPSW_PN_RESERVED_REG                     0xc022000: 0x0 
    CPSW_PN_CONTROL_REG                      0xc022004: 0x0 
    CPSW_INT_REVISION                        0xc001000: 0x6690a200 
    CPSW_INT_EOI_REG                         0xc001010: 0x0 
    CPSW_INT_INTR_VECTOR_REG                 0xc001014: 0x0 
    CPSW_INT_ENABLE_REG                      0xc001100: 0x0 
    CPSW_INT_ENABLE_CLR_REG                  0xc001300: 0x0 
    CPSW_INT_STATUS_REG                      0xc001500: 0x0 
    CPSW_INT_INTR_VECTOR_REG                 0xc001a80: 0x0 
    CPSW_ALE_MOD_VER                         0xc03e000: 0x294104 
    CPSW_ALE_STATUS                          0xc03e004: 0x80000c01 
    CPSW_ALE_CONTROL                         0xc03e008: 0x800000c4 
    CPSW_ALE_CTRL2                           0xc03e00c: 0x100000 
    CPSW_ALE_PRESCALE                        0xc03e010: 0x3d090 
    CPSW_ALE_AGING_CTRL                      0xc03e014: 0x141 
    CPSW_ALE_NXT_HDR                         0xc03e01c: 0x6061106 
    CPSW_ALE_TBLCTL                          0xc03e020: 0x3ff 
    CPSW_ALE_TBLW2                           0xc03e034: 0x0 
    CPSW_ALE_TBLW1                           0xc03e038: 0x0 
    CPSW_ALE_TBLW0                           0xc03e03c: 0x0 
    CPSW_ALE_UVLAN_MEMBER                    0xc03e090: 0x0 
    CPSW_ALE_UVLAN_URCAST                    0xc03e094: 0x0 
    CPSW_ALE_UVLAN_RMCAST                    0xc03e098: 0x0 
    CPSW_ALE_UVLAN_UNTAG                     0xc03e09c: 0x0 
    CPSW_ALE_STAT_DIAG                       0xc03e0b8: 0x0 
    CPSW_ALE_OAM_LB_CTRL                     0xc03e0bc: 0x0 
    CPSW_ALE_EGRESSOP                        0xc03e0fc: 0x0 
    CPSW_ALE_POLICECFG0                      0xc03e100: 0x0 
    CPSW_ALE_POLICECFG1                      0xc03e104: 0x800b0000 
    CPSW_ALE_POLICECFG2                      0xc03e108: 0x0 
    CPSW_ALE_POLICECFG3                      0xc03e10c: 0x0 
    CPSW_ALE_POLICECFG4                      0xc03e110: 0x0 
    CPSW_ALE_POLICECFG6                      0xc03e118: 0x0 
    CPSW_ALE_POLICECFG7                      0xc03e11c: 0x0 
    CPSW_ALE_POLICETBLCTL                    0xc03e120: 0x0 
    CPSW_ALE_POLICECONTROL                   0xc03e124: 0x80000000 
    CPSW_ALE_POLICETESTCTL                   0xc03e128: 0x0 
    CPSW_ALE_POLICEHSTAT                     0xc03e12c: 0x80000000 
    CPSW_ALE_THREADMAPDEF                    0xc03e134: 0x8003 
    CPSW_ALE_THREADMAPCTL                    0xc03e138: 0x0 
    CPSW_ALE_THREADMAPVAL                    0xc03e13c: 0x8000 
    

  • Hi,

    1. Can you do a CPSW register dump comparison between EVM and your device and just post the diff ?

    2. Sounds like an initialization issue maybe, can you post the output log of Ethernet Firmware ? It comes out on Main domain 3rd UART instance.

    3. Also post the Linux boot log.

    4. Which MII is this ? All ports or any particular port ?

    Regards

    Vineet

  • Since we are following up on email due to NDA requirements, closing this thread.

    Regards

    Vineet

  • Hi Vineet:

    When use static IP. at NDK change enableStaticIP = 1. Test 20 hours can not reproduce it.

    So we can change it to resolve mode.

    Best Regards!

    Han Tao

  • Thanks for confirming. closing the thread

    Regards

    Vineet