Part Number: TMS320C6455
Hi,
Customer connects EMIF with xilinx z7 instead of flash, is it possible to boot from z7? How to achieve this function? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320C6455
Hi,
Customer connects EMIF with xilinx z7 instead of flash, is it possible to boot from z7? How to achieve this function? Thanks!
Nancy,
We can only offer limited support on this device due to legacy nature of the device.
The EMIF boot on this device is documented in the Bootloader application notes here:
https://www.ti.com/lit/ug/spruec6g/spruec6g.pdf?ts=1619109196603
For EMIF NOR boot, the device appears to simply setup the EMIF peripheral and branch to the base address for executing code from the flash
EMIFA CE3 (0xB000 0000)
There are several useful threads discussing EMIF interface with FPGA and booting which you can refer:
https://e2e.ti.com/support/processors/f/processors-forum/467255/interface-c6455-to-fpga-via-emif
BIOS MCSDK here should also have tools and examples for this platform:
https://www.ti.com/tool/BIOSLINUXMCSDK
Hope this helps.
Regards,
Rahul