This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EXEVM: Running VSDK binary with A15 running on sysbios and A15 running on Linux in a similar manner

Part Number: TDA2EXEVM


Hi All,

I am running the VSDK binary ( Appimage and MLO ) on TDA2X board. Im running with A15 running on linux as well as A15 running on BIOS.

When i run A15 with BIOS, i flash only Appimage and MLO in SD card. And as soon as board boot-up it'll display the different use cases that can to run.

But when i use Linux on A15, 

  • I have to login as root
  • execute the shell script
  • and the run apps.out.

after the above steps it will display use-cases.

My question is, with A15 running Linux, it is possible to run use-cases ( similar to , when A15 running on BIOS) without above mentioned three steps .

Please let me know.

Regards,

Likhith