Hi ,
I am using AM335x processor with a custom board. I'm using staterware bootloader code, it is working with some changes in pinmuxing and is able to jump in to application. But when i add uart 0 in interrupt mode and timer interrupt, the interrupt is not handling properly.
I tested the code from the DDR its working fine . But if i load this into internal ram, its interrupt is not working and ISR is not called by system.
- When I was using bl_init.asm under "ti/AM335X_02_00_01_02/ bootloader/src/armv7a/cgt/", I was not able to get any interrupt it was jumping to some location which is system reserved.
- Then i changed the ".asm " file now I'm using " init.asm" under "ti/AM335X_02_00_01_01/system_config/armv7a/cgt/"
- Now whenever interrupt is generated it going into AbortHandler and infinite loop in exceptionhandler.asm file .
If any extra changes or extra function call is required in internal RAM (Bootloader) code for enabling interrupt, Please let me know what changes I need to do for the same asap.