Part Number: TDA4VM
Hi
TDA4VM Beta EVM can be run by using SDK SBL, but Alpha EVM cannot be done.
I found that the following log comment is different between these EVM.
Alpha EVM:Failed to set voltage to 800 mV for Slave:0x48, Res:0x0
Beta EVM:Successfully set voltage to 800 mV for Slave:0x48, Res:0x0
As far as I checked some E2E threads related to Alpha/Beta EVM, it seems that there is no difference between them.
What should I do to solve it?
Thanks and Best regards,
HaTa