This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CanSetBaudrateApi used as list in Can Driver

MCAL: Jacinto - 7

In Can schema file CanSetBaudrateApi is used as container :

<v:lst name="CanSetBaudrateApi">
 <a:da name="MAX" value="1"/>
 .......................
</v:lst>

According with autosar requirements this should be parameter