This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3359: Pixel Clock verification

Part Number: AM3359
Other Parts Discussed in Thread: SN75LVDS83B

I am using the Beaglebone Black with SDK Ver 3.03.00.004. I found an EMC issue that appears to be coming from the pixel clock at 65, 130 and 195Mhz. The LCD I am using is G104X1-L03 paired with the SN75LVDS83B IC. I measured the clock with my oscilloscope and it appears to be 65 Mhz which is the nominal frequency for the display. I just assumed that 130 and 195 MHz were harmonics from that clock, though I would like to confirm that.

My questions are:

How can I determine the pixel clock real frequency?

Where would the lcd driver likely be stored? I looked in the driver folder but could not find it.

Is there a way I can change the frequency through the command line without having to modify the driver?

Thanks