Other Parts Discussed in Thread: CC2500
I'm working with TI EVM5515 and TI transceiver cc2500.
I can read the cc2500 registers but can't write into them
can someone tell me what's wrong with the following write procedure?
Int8 SPI_write_reg (SPI_HwMode cs, Uint16 addr, Uint16* writedReg)
{
Uint16 spiStatusReg;
volatile Uint16 spiBusyStatus;
volatile Uint16 spiWcStaus;
Uint16 cmdBuffer[3];
int fnCnt;
Int8 status_byte;
cmdBuffer[0] = addr;
cmdBuffer[1] = writedReg[0];
CSL_FINS(CSL_SPI_REGS->SPICMD1, SPI_SPICMD1_FLEN, 1);
for(fnCnt = 0; fnCnt < 2; fnCnt++)
{
CSL_SPI_REGS->SPIDR2 = (Uint16)(cmdBuffer[fnCnt] <<0x08);
CSL_SPI_REGS->SPIDR1 = 0x0000;
CSL_SPI_REGS->SPICMD2 = (cs << CSL_SPI_SPICMD2_CSNUM_SHIFT)|
(SPI_WORD_LENGTH_8 << CSL_SPI_SPICMD2_CLEN_SHIFT)|
(CSL_SPI_SPICMD2_CMD_WRITE);
do
{
spiStatusReg = CSL_SPI_REGS->SPISTAT1;
spiBusyStatus = (spiStatusReg & CSL_SPI_SPISTAT1_BSY_MASK);
spiWcStaus = (spiStatusReg & CSL_SPI_SPISTAT1_CC_MASK);
}while((spiBusyStatus == CSL_SPI_SPISTAT1_BSY_BUSY) &&(spiWcStaus != CSL_SPI_SPISTAT1_CC_MASK));
}
status_byte = (Int8)CSL_FEXT(CSL_SPI_REGS->SPIDR1,SPI_SPIDR1_DATA)&0x00FF;
return (status_byte);
}
Thanks
Talmor