Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138,
Hi,
I am having a customized OMAPL138 board with customized UBL and u-boot code.
The customized UBL binary is been built out from the OMAP-L138_FlashAndBootUtils on ubuntu. Recently made some changes in UBL code, so I am planning to debug the UBL code using CCS utility to verify the functionality.
Below are the queries...
1. Now need SOP for debugging the customized UBL on CCS on the OMAPL138 board.
2. Installed CCS Version: 10.3.0.00007 on windows 10. I want to confirm that this version support OMAP L138, and moreover the UBL binary has been compiled on the Linux platform, but the CCS installed in the windows 10. Want to ensure that, this not create any dependency issue while debugging. (Read somewhere, this created dependency issue)
Thanks in advance...
MUTHUKUMAR V