This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTC_CVDD for unused RTC

There's a discrepancy in the data sheet.

Table 3-34 Unused RTC Signal Configuration says to connect RTC_CVDD to CVDD.

Section 5.2 Recommended Operating Conditions says that RTC_CVDD should have a 1.2V nominal voltage.

In the case of a 456 MHz device we will have CVDD = 1.3V (max 1.35V).

I believe we need to make one of the following changes:

  • For unused RTC connect RTC_CVDD to 1.2V (rather than CVDD). - OR -
  • In Recommended Operating Conditions perhaps we need to have 2 different specs, e.g. like RVDD

Can someone please confirm which is correct?  Bottom line, for unused RTC should I connect RTC_CVDD to 1.2V or 1.3V when using a 456 MHz device?

Thanks,
Brad