This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6A8168 pinout discrepancy between EVM and datasheet

I have a customer asking for clarification on pinout discrepencies between EVM schematics and datasheet: 

Pin

Data Sheet

EVM816 Schematic

AL22

RSV58

RSV59

AN21

RSV61

RSV60

AN30

EMAC[1]_RXER

MCTL_SDO

P32

RSV19

RSV17

P34

RSV17

X2USB

 

  • Hi,

    The EVM was originally done with the design pin names and EVM vendor had missed some pin names in the schematics to match the datasheet.

    Our EVM vendor will update this in the future schematics.

    Regards,

    yihe

     

  • Is this a problem also on the DM8168 EVM schematics?  The DM8168 reference design seems to use the same pin names with the datasheet saying something else and I just want to make sure our design is correct.

     

    Has the reference design schematic been updated to correct this?

     

    Thanks Bruce