i buy a TMS320C6211BGFN150 3.0, but i notice the pin number is different with datasheet, more than 256, what`s those addition pin use for? test pin?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i buy a TMS320C6211BGFN150 3.0, but i notice the pin number is different with datasheet, more than 256, what`s those addition pin use for? test pin?
Lidong
The package has an 20x20 pin array which, if fully populated would equal 400 pins. However, there is a 12x12 void in the center which is equivalent to 144 pins. This means that (400-144) only 256 pins are populated
Looking at the datasheet, all 256 pins are defined in the Terminal Functions section of the datasheet.
--Paul