This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6548: Reboot command is not working on AM6548 SR chip 2

Part Number: AM6548


Hi,

Reboot command is not working for SD Boot for SR2 chip with SDK 7.1ut from eMMC it is working properly.

I tried to remove the 1.8V SDHC property from linux device tree but that didnt solve the issue . I received the SDHCP Crash logs on mounting during boot time.

I can see this issue is in the known bugs in release notes if there is any patch available pls share the same.

Thanks,

Sarfaraz