Other Parts Discussed in Thread: TVP5146, TVP5150
Hi, all
We got Appro IPNC Software v2.6 which support TVP5146 Sensor YUV input.
Our board is using TVP5150 which is simple to TVP5146, I modify the source code under ipnc/av_caputer/framework/drv/usermod/imgs_TVP514X/drv_imgs_TVP514X.c,
operate the I2C operation to TVP5150 such as the TVP5146 does. Then I run the ipnc application, I can successfully boot up the board and access the website of the board ,
login admin to operate, but the video is not right.
The video is very bad, is distorted, sometime the upper is moving right while the lower is moving left.
I have no idea why this happen.
Would someone give me some help.
Thansk
David