Hi,
I'm trying to create a new project with the EVMC6657 board. I'd like to implement a simple telnet program on the EVMC6657 to test the Ethernet connection. I see the option to add a telnet instance in SYS/BIOS. However, I cannot compile the project, I get linker errors such as this :
first referenced
symbol in file
--------- ----------------
Convert_CoreLocal2GlobalAddr C:\ti\pdk_c665x_2_0_16\packages\ti\transport\ndk\nimu\lib\c6657\c66\release
Is there a tutorial or an example project for that? I spent a lot of time and I couldn't find anything. I installed the C6657 SDK and C665x PDK.
Regards
Benjamin