Part Number: AM3352
Hi Texas team,
We have a custom board with an AM3352 and I was checking some changes that we made across the last years in this project and noted that we disrespect a datasheet parameter after changing a 24MHz crystal (reduced footprint for improving placement). We didn't realize that doing that we changed the ESR of the device due to the small package.
We never received any negative reports after this change. But am I wondering what are the expected behaviors of not respecting the ESR specification of an oscillator circuit? We did some SI analysis and noted a slower star-up time, but nothing that matters, from 250us to 600us. But after the circuit is in a steady state the values and measures are equals.
I searched for more cases with this same question and the best approach was founded on this topic but not finish it. e2e.ti.com/.../tms320f28377s-about-crystal-equivalent-series-resistance-esr-requirements
My main question is, could this affect the MPU in some strange behavior (PLL not fixing, drift frequencies, or anything worse)? Or it's more about efficiency and start-up timing?
To let you guys know my specific case we have:

The ESR from most manufacturers for the size (2.5x3.2mm) that we updated is around 60Ohms.
Our older board have an crystal with ESR max < 50 and; Our updated board with ESR max < 60.
Our capacitance used in both cases are 18pF, We noted that reducing that to 12pF the start-up time is improved (reduced).