This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Survey SOC for projector

Other Parts Discussed in Thread: WL1837

Dear Sir,

i have new projector project request below feature.

1. android 9 + BT+WIFI

2. LVDS 1080p supporting

3. WIFI : 802.11 a/b/g/n 2.5G & 5G

many thanks if any processor or SOC suggestion. thanks.

Regards,

bard 

  • Hi Bard,

    A few questions to clarify the best TI Wi-Fi part.

    1. Is this projector a portable mini projector that uses batteries, or is it a line-powered device?

    2. When you mention "Android 9", do they mean that they want to have Android 9 run on the SoC, or they want to be able to connect to an Android device using BT and Wi-Fi?

    3. Does the customer already have a processor that will do the 1080p decoding, or does that have to be done through the SoC we provide?

    I'm thinking that if the customer wants to run Android on a SoC + BT + Wi-Fi solution we provide, the solution will look like a AM65x device with a WL1837. The WL1837 has the needed Wi-Fi features + BT and BLE support.

    Regards,

    Michael

  • Hi Bard,


    A few questions to clarify the best TI Wi-Fi part.
    1. Is this projector a portable mini projector that uses batteries, or is it a line-powered device?
    Battery 3 hours after full charging. 

    2. When you mention "Android 9", do they mean that they want to have Android 9 run on the SoC, or they want to be able to connect to an Android device using BT and Wi-Fi?
    Customer expect the SoC can run Android 9.

    3. Does the customer already have a processor that will do the 1080p decoding, or does that have to be done through the SoC we provide?
    Customer hope SoC can finish this task.

    I'm thinking that if the customer wants to run Android on a SoC + BT + Wi-Fi solution we provide, the solution will look like a AM65x device with a WL1837. The WL1837 has the needed Wi-Fi features + BT and BLE support.
    Regards,

  • Hi,

    For Wi-Fi, using the WL1837 still makes sense given the info provided. Do note that this will result in a two-chip solution, one for Wi-Fi + BT and one for the man MPU.

    I will reassign this thread to the processors team, who can assist with the MPU selection.

    Regards,

    Michael

  • Hello Bard,

    Currently, we do not support Android on our devices. I would recommend checking with third party for further support and here is the link: https://witekio.com/software-accelerators/board-support-package-bsp-development/. The Jacinto team has Android SDK available for several devices:
    1. https://www.ti.com/tool/PROCESSOR-SDK-AM57X
    2. https://www.ti.com/tool/PROCESSOR-SDK-AM65X 

    Regards,
    Krunal