Other Parts Discussed in Thread: TMS320C5505
Page 63 of the TMS320C5505 datasheet (rev B) indicates the input leakage current of any pin can be as high as +/- 5uA. Additionally, page 128 specifies an analog input impedance of 1 M-ohm. When configured as an analog input, do both of these parameters need to be taken into account when calculating the accuracy of the input signal measurement incident to a given GPAIN pin, or are they dependent on the configuration of the pin?
Thanks - AM