Part Number: TDA4VM
Hi,
My working environment is qnx+rtos on the tda4 board, we want to get information (such as CPU utilization, memory size) about the running program?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Memory and CPU usage can be seen using different QNX utilities. The QNX utilities are documented online at qnx.com
The QNX "top" utility can be used to show CPU usage.
20 processes; 86 threads;
CPU states: 0.0% user, 0.0% kernel
CPU 0 Idle: 99.9%
CPU 1 Idle: 99.8%
Memory: 4096M total, 2519M avail, page size 4K
PID TID PRI STATE HH:MM:SS CPU COMMAND
1 14 10 Run 0:00:00 0.04% kernel
221204 1 10 Rply 0:00:00 0.02% top
11 2 21 Rcv 0:00:00 0.00% io-pkt-v6-hc
5 2 10 NSlp 0:00:00 0.00% random
6 1 24 Rcv 0:00:00 0.00% devc-seromap
12300 9 10 Rcv 0:00:00 0.00% io-usb-otg
1 3 10 Rcv 0:00:00 0.00% kernel
1 11 10 Rcv 0:00:00 0.00% kernel
20494 1 10 Rcv 0:00:00 0.00% tisci-mgr
36880 1 10 Rcv 0:00:00 0.00% tiipc-mgr
Min Max Average
CPU 0 idle: 99% 99% 99%
CPU 1 idle: 99% 99% 99%
Mem Avail: 2519MB 2519MB 2519MB
Processes: 20 20 20
Threads: 86 86 86
The QNX "pidin" utility can be used to show different view of memory
The "pidin in" option will show overall system usage
CPU:AARCH64 Release:7.0.4 FreeMem:2519MB/4096MB BootTime:Jan 01 00:00:00 GMT 1970 Actual resident free memory:2520Mb Processes: 20, Threads: 86 Processor1: 1092604032 Cortex-A72 2000MHz FPU Processor2: 1092604032 Cortex-A72 2000MHz FPU
The "pidin mem" , will show memory used by all processes, use"pidin -P <process name> mem", to look at memory usage by a specific process
J7EVM@QNX:/# pidin -P procnto-smp-instr mem
pid tid name prio STATE code data stack
1 1 /procnto-smp-instr 0f RUNNING 0 0 480(480)
1 2 /procnto-smp-instr 0f READY 0 0 480(480)
1 3 /procnto-smp-instr 10r RUNNING 0 0 8192(8192)
1 4 /procnto-smp-instr 1r RECEIVE 0 0 512K(512K)
1 5 /procnto-smp-instr 10r CONDVAR 0 0 8192(8192)
1 6 /procnto-smp-instr 10r CONDVAR 0 0 8192(8192)
1 7 /procnto-smp-instr 255r RECEIVE 0 0 8192(8192)
1 8 /procnto-smp-instr 255r RECEIVE 0 0 8192(8192)
1 9 /procnto-smp-instr 255r RECEIVE 0 0 8192(8192)
1 10 /procnto-smp-instr 255r RECEIVE 0 0 8192(8192)
1 11 /procnto-smp-instr 10r RECEIVE 0 0 8192(8192)
1 12 /procnto-smp-instr 10r RECEIVE 0 0 8192(8192)
1 13 /procnto-smp-instr 10r RECEIVE 0 0 8192(8192)
1 14 /procnto-smp-instr 10r RECEIVE 0 0 8192(8192)
1 15 /procnto-smp-instr 21r RECEIVE 0 0 8192(8192)
procnto-smp-instr @ffffff8060045000 689K 108K
Regards,
kb
Hi,
The vision apps framework provides examples of performance measurement of the R5 / DSP cores. See APIs at Vision Apps User Guide: Performance statistics reporting APIs.
When running Vision Apps demos from the command line on QNX, at run time there is a "p" option to print off performance statistics.

Regards,
kb