I have read through the datasheet and the TRM for the TMS320C6A816x and unfortunately they appear to be in conflict for the maximum data throughput on the GPMC. What is the maximum possible burst data throughput via the GPMC? Does it depend on whether the target device is Asynchronous or Synchronous? Ideally, I would prefer to use a Synchronous port as my target will be an FPGA. The TRM appears to imply that with proper register configuration I could get a burst transfer rate of 125MHz x 2bytes per transfer. The data sheet seems to imply that the max rate would b 62.5 MHz x 2 bytes per transfer. Which is correct?
Is there any sample code or discussion about how to configure a bank on the GPMC for maximum possible transfer rate?
TIA,
B.J.