Other Parts Discussed in Thread: OMAP3530
I'm having some difficulty getting the Gstreamer built using Ubuntu 10.04(host) onto my OMAP3 C4 rev. BeagleBoard running Ubuntu 10.10.
When I start the make process all seems to go well for a while, but then I get the following error message. However no matter how I try to install
ZLIB this error keeps coming up. Below I show how I finally tried to install zlib using the instructions on the linuxfromscratch.org
(http://www.linuxfromscratch.org/lfs/view/development/chapter06/zlib.html) website.
I also tried to set the environment varibable with export CPPFLAGS="-I/usr/bin/ -I/usr/include" and LDFLAGS="-L/usr/bin -L/usr/include" before running the make operation,
even added /usr/lib and /usr/include to my PATH
I have Gstreamer gst-ti-plugin-full-1.02.00 and ti tool DVSDK dvsdk_omap3530-evm_4_01_00_09
ee:~/share/zlib-1.2.5$ whereis zlib.h
zlib: /usr/include/zlib.h /usr/share/man/man3/zlib.3
ee:~/share/zlib-1.2.5$ whereis libz
libz: /usr/lib/libz.a /usr/lib/libz.so
I'm out of ideas and completely stick now, so anything that can be suggested will certianly help.
checking if /home/michaels8/CodeSourcery/Sourcery_G++_Lite2009q1-203//bin/arm-none-linux-gnueabi-g++ supports -c -o file.o... yes
checking whether the /home/michaels8/CodeSourcery/Sourcery_G++_Lite2009q1-203//bin/arm-none-linux-gnueabi-g++ linker (/home/michaels8/CodeSourcery/Sourcery_G++_Lite2009q1-203/arm-none-linux-gnueabi/bin/ld) supports shared libraries... yes
checking dynamic linker characteristics... GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
checking whether stripping libraries is possible... yes
appending configuration tag "F77" to libtool
checking for ANSI C header files... (cached) yes
checking assert.h usability... yes
checking assert.h presence... yes
checking for assert.h... yes
checking for unistd.h... (cached) yes
checking zlib.h usability... no
checking zlib.h presence... no
checking for zlib.h... no
configure: error: zlib.h was not found
*** You must first install zlib (libz) before you can build this package.
*** If zlib is already installed, you may need to use the CPPFLAGS
*** environment variable to specify its installed location, e.g. -I<dir>.
make[4]: *** [id3tag.configure] Error 1
make[4]: Leaving directory `/home/michaels8/BeagleBoard/Gstreamer/gst-ti-plugin-full-1.02.00/opensource_build'
make[3]: *** [base] Error 2
make[3]: Leaving directory `/home/michaels8/BeagleBoard/Gstreamer/gst-ti-plugin-full-1.02.00/opensource_build'
make[2]: *** [.base] Error 2
make[2]: Leaving directory `/home/michaels8/BeagleBoard/Gstreamer/gst-ti-plugin-full-1.02.00/opensource_build'
make[1]: *** [opensource_build] Error 2
make[1]: Leaving directory `/home/michaels8/BeagleBoard/Gstreamer/gst-ti-plugin-full-1.02.00'
make: *** [all] Error 2
michaels8@SMFeelab2:~/BeagleBoard/Gstreamer/gst-ti-plugin-full-1.02.00$