Part Number: TDA4VM
What are the steps for executing linux DSS on SDK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
What are the steps for executing linux DSS on SDK?
Note : Please ensure that the DSS module is working fine on the RTOS side (i.e., Please run a vision_apps demo in the RTOS SDK which uses the display)
Please follow the below steps to run the DSS (Display SubSystem) hardware on Linux using tidss driver
Step 1 : Disable all the DSS related macros in ${PSDKRA}/vision_apps/platform/j721e/rtos/common/app_cfg_mcu2_0.h [i.e., ENABLE_DSS_SINGLE or ENABLE_DSS_DUAL (ENABLE_DSS_EDP, ENABLE_DSS_HDMI or ENABLE_DSS_DSI)]
Step 2 : Clean build vision_apps as shown below
cd ${PSDKRA}/
make vision_apps_scrub
make vision_apps -j
Step 3 : Copy the file system into the SD using below command
make linux_fs_install_sd
Step 4 : In the Linux SDK (i.e., PSDKLA), remove the dss related components that are disabled (i.e., serdes_wiz4, mhdp, dss, main_i2c1) , from the file ${PSDKLA}/board-support/linux-5.10.120+gitAUTOINC+95b90aa828-g95b90aa828/arch/arm64/boot/dts/ti/k3-j721e-vision-apps.dts
Step 5 : Build the vision_apps overlay using below command
cd ${PSDKLA}/
make linux-dtbs
Step 6 : Copy the file k3-j721e-vision-apps.dtbo present at ${PSDKLA}/board-support/linux-5.10.120+gitAUTOINC+95b90aa828-g95b90aa828/arch/arm64/boot/dts/ti/ to /media/${USER}/rootfs/boot/ and replace the existing file.
Step 7 : Insert the SD card into the EVM and boot
Step 8 : Before Login, you would see that the display is detected on the monitor.
Step 9 : Login as root and do the below command if the weston service is running
killall weston
Step 10 : In order to display a pattern on the display, you could run the below command
modetest -M tidss -s 39@37:1920x1080
Note : Please check if the port ID is 39 on your device using below command
modetest -M tidss | grep connected
Regards,
Nikhil