Part Number: MCU-PLUS-SDK-AM243X
Tool/software:
Hi, AM243x MCU SDK includes an FSI internal loopback example, but I would like to test an external loopback using 2 boards. How can I do it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MCU-PLUS-SDK-AM243X
Tool/software:
Hi, AM243x MCU SDK includes an FSI internal loopback example, but I would like to test an external loopback using 2 boards. How can I do it?
Recommended to try first 1-device loopback
Software:
Hardware:
Device 1 (J16) <-> Device 2 (J16)
RX0_CLK <-> TX0_CLK
TX0_CLK <->RX0_CLK
GND <-> GND (both lines of ground)
RX0_D0 <-> TX0_D0
TX0_D0 <-> RX0_D0
Alternative (recommended) use "Fast serial interface (FSI) adapter board evaluation module" daughter card on top of LP.

Software:
Hardware:
Device 1 (J7 Rev C) <-> Device 2 (J16)
RX0_CLK <-> TX0_CLK
TX0_CLK <-> RX0_CLK
GND <-> GND (both lines of ground)
RX0_D0 <-> TX0_D0
TX0_D0 <-> RX0_D0
Alternative (recommended) use "Fast serial interface (FSI) adapter board evaluation module" daughter card on top of LP. AM243x EVM connects to this daughter card with jumper cables.



*NOTE the Mezzanine board on the https://www.ti.com/tool/TMDS243EVM in the picture is unrelated to the FSI setup