Other Parts Discussed in Thread: AM62L, AM62P
Tool/software:
Hi TI Experts,
Do you have any suggestion on configuring the bootmode pins for alternate functions? I am using the bootmode resistors + buffers to configure the SOC boot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Board Designers,
the below diagram includes the following
Connection of bootmode resistors to the buffer input and connection of the buffer output through 1K series resistor is shown in the below diagram.
The bootmode pin from the SOC can be connected to the alternate function through a 0R resistor.
The 0R resistor can be used to isolate the alternat functions to test the bootmodes.

SOC_Bootmode_Configuration.pdf
Regards,
Sreenivasa
Hi Board Designers,
Additional inputs
Connecting bootmode pins directly to supply
They should never connect any bidirectional IO directly to the power rail. There is a good chance the device output buffer would be damaged if the pin is connected directly to 3.3V and the output buffer is accidently driven low.
The N-channel FET may be damaged or the metal connecting the FET to the pin or VSS. Anytime you damage something in a device with these small geometries, the damage is very likely to spill over to adjacent circuits. So no guarantee the output buffer is the only thing damaged.
MCU_PORz or RESETSTATz to control bootmode buffers
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1352163/am67a-mcu_porz-or-resetstatz-to-control-bootmode-buffers/5160825?tisearch=e2e-sitesearch&keymatch=bootmode%252520buffer#5160825
Buffer on SOP boot mode pins
https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1206852/am2634-buffer-on-sop-boot-mode-pins/4558332?tisearch=e2e-sitesearch&keymatch=bootmode%2520buffer#4558332
BOOTMODE Pin Sample Timing
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1070744/dra821u-bootmode-pin-sample-timing?tisearch=e2e-sitesearch&keymatch=bootmode%2525252525252520buffer#
Regards,
Sreenivasa
Hi Board Designers,
Additional inputs specific to AM62L
RESETSTATz - is the reset status output available for AM62L devices and can be used for latching of the bootmode configuration.
AM62L supports reduced pin count and Fullpin count boot modes.

The implementation above is similar and can be followed.
Regards,
Sreenivasa
Hi Board Designers,
Boot mode configurations on the EVM/SK
AM64x

AM243x ALX

AM62x

AM62A

AM62P boot mode inputs

AM62L

Regards,
Sreenivasa