This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP35x TO AM37x Hardware Migration Guide



Hi all,

In OMAP35x TO AM37x Hardware Migration Guide (http://processors.wiki.ti.com/index.php/OMAP35x_To_AM37x_Hardware_Migration_Guide), it is mentioned that Display sub system data lines need to be muxed to SYSBOOT pins for operating AM37x in two modes (PCLK <60 MHz & PCLK >60 MHz).

It is mentioned as "Backward compatibility is maintained if your pixel clock on DSS interface is <= 60 MHz. But if your pixel clock is higher, 60< PCLK <= 75 MHz, you would need to use the High Speed Mode pinmux scheme. For all new AM37x designs, High Speed Mode pinmux scheme should be used. "

In our new design, we are making use of both small size LCD and HDMI moniter for display.

LCD pclk - less than 60 MHz

HDMI pclk - greater than 60 MHz

I have designed in schematics with both LCD & HDMI transceiver data lines configured in high speed mode pinmux scheme. Is that okay?

i.e d0-d5 (display side) --> d18-d23 (omap side)

    d6-d17(display side)--> d6-d17 (omap side)

  d18-d23(display side)-->sysboot(0,1,3,4,5,6)

Since I am not sure that LCD with pixel clock less than 60 MHz work in high speed mode pinmux scheme.

Thanks,

Karthik