This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CMEM Fail!!



Hi 

   When Run 138, CMEM ERROR appear.

   DVSDK 4.01 Memory:256M  and CMEM Not changed, it is default!

    the log is:

CMEMK module: built on Mar 17 2014 at 19:16:08
Reference Linux version 2.6.33
File /work/dvsdk/linuxutils_2_25_05_11/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c
CMEM Range Overlaps Kernel Physical - allowing overlap
CMEM phys_start (0xc2000000) overlaps kernel (0xc0000000 -> 0xc4000000)
CMEMK Error: Failed to request_mem_region(0xc2000000, 18874368)
FATAL: Error inserting cmemk (/lib/modules/2.6.33-rc4/kernel/drivers/dsp/cmemk.ko): Bad address

    Why? who can help me ?

    Thanks.