In section 4.23 of SPRUGV8E, DDR3 Memory Controller Registers, the DDR_PHY_CTRL_1 register is described. The three LOCAL_ODT fields are each two bits, but there is no explanation of what the four possible settings do for each field. In particular, the RD_LOCAL_ODT field (bits 9-8) defaults to 0x01, which I believe means 'Full Thevenin Termination'. I assume that setting this field to 0x00 disables the termination, but what termination do the 0x10 and 0x11 settings provide?
Thanks, John.