Other Parts Discussed in Thread: TPS51200, AM3358
Hello,
My AM335x is connected to a single 16bit-DDR3 chip, the Vtt is generated by a voltage divider.
My system starts up and boots linux just fine using the beagleboneblack DDR3 u-boot settings.
Now I'd like to check and optimize my DDR3 settings but the software leveling fails.
I follow the instructions from the wiki: http://processors.wiki.ti.com/index.php/AM335x_DDR_PHY_register_configuration_for_DDR3_using_Software_Leveling
But the S/W leveling only reports zeros:
[CortxA8]
Enter the PHY_INVERT_CLKOUT value (0 or 1) from the spreadsheet
1
Enter the Seed RD_DQS_SLAVE_RATIO Value in Hex to search the RD DQS Ratio Window
80
Enter the Seed FIFO_WE_SLAVE_RATIO Value in Hex to search the RD DQS Gate Window
40
Enter the Seed WR_DQS_SLAVE_RATIO Write DQS Ratio Value in Hex to search the Write DQS Ratio Window
F8
***************************************************************
The Slave Ratio Search Program Values are...
***************************************************************
PARAMETER MAX | MIN | OPTIMUM | RANGE
***************************************************************
DATA_PHY_RD_DQS_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_FIFO_WE_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_WR_DQS_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_WR_DATA_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
***************************************************************
rd_dqs_range = 0
fifo_we_range = 0
wr_dqs_range = 0
wr_data_range = 0
Optimal values have been found!!
***************************************************************
The Slave Ratio Search Program Values are...
***************************************************************
PARAMETER MAX | MIN | OPTIMUM | RANGE
***************************************************************
DATA_PHY_RD_DQS_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_FIFO_WE_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_WR_DQS_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
DATA_PHY_WR_DATA_SLAVE_RATIO 0x000 | 0x000 | 0x000 | 0x000
***************************************************************
===== END OF TEST =====
This is similar to this post: https://e2e.ti.com/support/arm/sitara_arm/f/791/t/379997#pi316653=3
But I have not GPIO to switch Vtt.
Please find attached a spreadsheet with all my settings (SDRAM_TIM_xxx) and calculations (ratio search)
Memory: MT41K128M16JT-125:K FBGA CODE D9PTK datasheet: http://www.micron.com/~/media/documents/products/data-sheet/dram/ddr3/2gb_1_35v_ddr3l.pdf
Is there a way to modify the GEL file or procedure so I can do DDR3 SW/ leveling?
Regards,
Lo2