Other Parts Discussed in Thread: ASH
Hi forums,
I am currently trying to mount the ubi.img on mtd9 but i get the following error. any suggestions and solutions are welcome.
log is as below
root@am437x-evm:/# ls
bin etc lib opt sbin tmp var
boot home media proc srv ubi.img www
dev include mnt run sys usr
root@am437x-evm:/# mtdinfo /dev/mtd9
mtd9
Name: NAND.file-system
Type: nand
Eraseblock size: 262144 bytes, 256.0 KiB
Amount of eraseblocks: 2008 (526385152 bytes, 502.0 MiB)
Minimum input/output unit size: 4096 bytes
Sub-page size: 1024 bytes
OOB size: 224 bytes
Character device major/minor: 90:18
Bad blocks are allowed: true
Device is writable: true
root@am437x-evm:/# ubiformat /dev/mtd9 -f ubi.img -s 1024 -O 2048
ubiformat: mtd9 (nand), size 526385152 bytes (502.0 MiB), 2008 eraseblocks of 2s
libscan: scanning eraseblock 2007 -- 100 % complete
ubiformat: 139 eraseblocks have valid erase counter, mean value is 1
ubiformat: 1869 eraseblocks are supposedly empty
ubiformat: warning!: only 139 of 2008 eraseblocks have valid erase counter
ubiformat: erase counter 0 will be used for all eraseblocks
ubiformat: note, arbitrary erase counter value may be specified using -e option
ubiformat: continue? (y/N) y
ubiformat: use erase counter 0 for all eraseblocks
ubiformat: warning!: VID header and data offsets on flash are 4096 and 8192, wh6
ubiformat: use new offsets 2048 and 4096? ubiformat: continue? (y/N) y
ubiformat: use offsets 2048 and 4096
ubiformat: error!: file "ubi.img" is too large (576061440 bytes)
error 0 (Success)
root@am437x-evm:/#
Regards
-Ash