Other Parts Discussed in Thread: AM5728, AM3358
Hi,
Can the sysboot resistor values of AM335X series be of the value 220K.
I have 220K in stock at present. It is 100K on BBB.
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The answer to this question is system dependent and needs to be evaluated on a per system, per pin basis. The voltage applied to the SYSBOOT input must be above the min VIH or below the max VIL when the respective reset input rises above its max VIL. Each external pull resistor will need to be sized such that it pulls the respective SYSBOOT input to the appropriate level in the time provided by the shortest reset pulse. You also need to consider the effect of leakage current through all devices attached to each SYSBOOT signal. This includes worst case input leakage of the input buffer plus any leakage through internal resistors.
Regards,
Paul
Hi Paul,
What are the max VIL levels for the Sysboot? I'm at about 1V, and seem to be OK, but don't want to run into trouble if this is marginal. We're running with those at 3.3V.