This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: SYSBOOT pins connection

Part Number: AM3358


There are 16 pins that are used to select booting sequence of AM3358 (R1~R4, T1~T4, U1~U4, V2~V5). I am using 100K resistors to pull the pins to high or low. Since the booting sequence is fixed in my design, can I just use straight connection to 3.3V or GND instead of using resistors to configure booting sequence?

Thank you.