This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA744: Uboot some time will booting fail

Part Number: DRA744


Tool/software: Linux

Hi,

I have booting the DRA744 on uboot process.

Some time will stop the boot process that I have check the power sequence and power of PMIC is ok.

The related log as below,

Could any one please tell me how can I debug this issue?

Thank you.

U-Boot SPL 2014.07 (May 09 2017 - 17:39:04)

DRA752-GP ES1.1

IODELAY: Isolation of Device IOs failed

ti_i2c_eeprom_init failed 1

===lisa_map_dra7_1536MB===

===EMIF-(1) Interface Setting===

===Ram Size = 0x0 ===

Use emif1_ddr3_532_mhz_1cs

===EMIF-(2) Interface Setting===

===Ram Size = 0x0 === SDRAM: identified size not same as expected size identified: 4 expected: 40000000