Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3359
Tool/software: TI-RTOS
Goodmorning,
I'm using a BegleBone Black with TI-RTOS "ti-processor-sdk-rtos-am335x-evm-04.02.00.09-Windows-x86-Install.exe". I've tried both the boot from SD card and UART, but the program always get stuck as follow:
StarterWare Boot Loader BOARDInit status [0x0] SoC : [AM335X] Core : [A8] Board Detected : [BEAGLEBONEBLACK] Base Board Revision : [UNKNOWN] Daughter Card Revision: [UNKNOWN] Please transfer file with XMODEM protocol... CCCCCCCCCCCCCCCCC Xmodem received 899072 bytes Copying application image from UART to RAM is done Jumping to StarterWare Application...
The steps that I followed are the following
- As explained by the document "processors.wiki.ti.com/index.php/Rebuilding_The_PDK" I've generated a simple GPIO app.
- I've generated the MLO file and app with the following post-scripts command:
@echo 'Transform the MMCSD from .bin to MLO' "C:/ti/pdk_am335x_1_0_9/packages/ti/starterware/tools/ti_image/tiimage.exe" 0x402F0400 UART "C:/ti/pdk_am335x_1_0_9/packages/ti/starterware/binary/bootloader/bin/am335x-evm/gcc/bootloader_boot_uart_a8host_release.bin" "${BuildDirectory}/MLO" @echo 'Transform the application from .out to .bin' "C:/ti/gcc-arm-none-eabi-6-2017-q1-update/arm-none-eabi/bin/objcopy.exe" "${BuildDirectory}/${BuildArtifactFileBaseName}.out" "${BuildDirectory}/${BuildArtifactFileBaseName}.bin" @echo 'Transform the application from .bin to app' "C:/ti/pdk_am335x_1_0_9/packages/ti/starterware/tools/ti_image/tiimage.exe" 0x80000000 NONE "${BuildDirectory}/${BuildArtifactFileBaseName}.bin" "${BuildDirectory}/app" - Copy the MLO file in the SDcard and then transfer the app file with teraterm (XMODEM mode).
What are the possible causes that prevent the app to start?
Thank you.