Part Number: AM3354
Hi,
Our customer is using TSC_ADC to control touchscreen.
Sometimes FSM_BUSY occurs and TSC_ADC hangs.
After the occurrence of FSM_BUSY, if the following processing is executed, it returned normally but is it correct as processing?
① Set the enable bit of the CTRL register to 0.
② Resetting the STEPENABLE register
③ Set the enable bit of the CTRL register to 1.
In the answer of the following e2e site, the answer was that the recovery process had only hardware reset.
e2e.ti.com/.../555302
http://e2e.ti.com/support/arm/sitara_arm/f/791/t/596863
Best Regards,
Shigehiro Tsuda